Displaying results in English. Change.

Select languages to include in search results






Challenges on the Road to an Offshore HVDC Grid

Industries and utilities > Power T&D Solutions > HVDC > HVDC Light

... systems with 70 km long DC link between rectifier and inverter. ... that the galvanic barrier also will prevent DC potential to enter the AC system, so ...

Adobe Acrobat

Updated: 2009-11-04

B4-104

Industries and utilities > Power T&D Solutions > HVDC > HVDC Classic

... one for switches, two for the DC filter capacitor banks, and one for the DC PLC capacitor ... To keep the AC yard at Jingzhou converter station of ...

Adobe Acrobat

Updated: 2004-08-30

HVDC GRIDS FOR OFFSHORE AND ONSHORE ...

Industries and utilities > Power T&D Solutions > HVDC > HVDC Light

... check in service ▪ Proven Power electronic design similar to converter technology ... investment cost o Decrease AC-DC conversion losses ...

Adobe Acrobat

Updated: 2011-12-07

Recent evolution in classic HVDC

Industries and utilities > Power T&D Solutions > HVDC > HVDC Classic

... Keywords: AC filters, Capacitor-Commutated Converter, Control systems, DC filters, Development, Garabi, HVDC converters ...

Adobe Acrobat

Updated: 2003-09-09

Three Gorges - Shanghai HVDC: Reinforcing Interconnection ...

Industries and utilities > Power T&D Solutions > HVDC > HVDC Classic

... even during a case of partial loss of DC line insulation. 2. Reactive Power and AC Filters Since Yidu converter station is directly connected to Three ...

Adobe Acrobat

Updated: 2006-11-06

— HVDC Light® The original VSC technology

Industries and utilities > Oil & Gas Solutions > Offshore Production [Classic] > Electrical > Integrated Project Solutions [Classic] > HVDC Light [Classic]

... energy trade City center infeed, energy tra- de, controllability DC links in AC grids, weak ... Direct voltage per converter, kV 31.8 300 142 400 ...

Adobe Acrobat

Updated: 2017-08-25

Electrical supply for offshore installations made possible by ...

Industries and utilities > Power T&D Solutions > HVDC > HVDC Light

... possibly minor changes of the DC voltage level. ... operation at much higher operating AC voltages (up ... A transformer between the inverter and motor ...

Adobe Acrobat

Updated: 2005-04-05

Case Study of a Multi-Infeed HVDC System

Industries and utilities > Power T&D Solutions > HVDC

... in one HVDC link was increased while dc currents in ... feeders to the load area close to inverter bus and ... trip of single/double circuits AC line feeders ...

Adobe Acrobat

Updated: 2009-04-29

HVDC Light An excellent tool for City Center Infeed

Industries and utilities > Power T&D Solutions > HVDC > HVDC Light

... can also utilize existing AC overhead lines, and by converting to DC, power transfer capability ... is based on voltage source converter technology ...

Adobe Acrobat

Updated: 2005-04-05

1 Power System Reliability and Transfer Capability ...

Industries and utilities > Power T&D Solutions > HVDC > HVDC Light

... is realized by designating only one converter controlling the ... A constant dc voltage control gives a ... Controlling ac voltage or reactive power, however ...

Adobe Acrobat

Updated: 2007-07-19