| | | | |
 | English - 0,75MB
| Movie 2005-06-20 | |
 |
Doc No: IWM/004 Document kind: Movie Language: English Size: 0,75MB Expected download time: 1 minutes (speed: 56Kb) Published: 2005-06-20 Revision: A File type: vcm Summary: This module looks at setting an analog output to flow rate. Topics discussed are operations, register addresses (app. array, register), and checking the successful operation of AO.
|
 | English - 0,87MB
| Movie 2005-06-20 | |
 |
Doc No: IWM/001 Document kind: Movie Language: English Size: 0,87MB Expected download time: 2 minutes (speed: 56Kb) Published: 2005-06-20 Revision: A File type: vcm Summary: This module is for the diagnostics on the Btu 8000. Topics are initiating the diagnostics, what happens, and looking at the results of the diagnostics. Running the diagnostics will help identify problems in the Btu 8000.
|
 | English - 2,07MB
| Movie 2005-06-20 | |
 |
Doc No: IWM/006 Document kind: Movie Language: English Size: 2,07MB Expected download time: 5 minutes (speed: 56Kb) Published: 2005-06-20 Revision: A File type: vcm Summary: This is a combination of two other modules with more detail. Discussion includes hardware and software involved in complete setup of the AO. Topics are AO modules and pin outs, calibration of the AO with a multimeter, operations application, register addresses (app. array, register), and rang of the output.
|
 | English - 0,63MB
| Movie 2005-06-20 | |
 |
Doc No: IWM/003 Document kind: Movie Language: English Size: 0,63MB Expected download time: 1 minutes (speed: 56Kb) Published: 2005-06-20 Revision: A File type: vcm Summary: With the Btu 8000 one of the basic pieces of knowledge needed to understand the "inner workings" is to be able to identify peaks on the chromatogram. This module attempts to give the beginning of this knowledge. The chromatogram is divided into detector 1 and detector 2. Peaks on each detector are discussed along with the order and some background about this order.
|
 | English - 0,73MB
| Movie 2005-06-20 | |
 |
Doc No: IWM/002 Document kind: Movie Language: English Size: 0,73MB Expected download time: 1 minutes (speed: 56Kb) Published: 2005-06-20 Revision: A File type: vcm Summary: This module discusses setting up a trend for the battery voltage and the charger. There is information about the register addresses, trend setup, saving the setup, and sending the file to the XFC.
|
 | English - 0,00MB
| Movie 2007-11-20 | |
 |
Doc No: Movie001 Document kind: Movie Language: English Size: 0,00MB Expected download time: 0 seconds (speed: 56Kb) Published: 2007-11-20 Revision: A File type: html Summary: LevelMaster Guided Image
|
 | English - 5,67MB
| Movie 2007-02-01 | |
 |
Doc No: WMP001 Document kind: Movie Language: English Size: 5,67MB Expected download time: 13 minutes (speed: 56Kb) Published: 2007-02-01 Revision: A File type: wmv Summary: This module will describe different post processing options when performing a manual peak find with the NGC8206. Post processing is a quick technique for changing parameters and seeing immediate results without running a complete 5 minute single cycle.
|
 | English - 1,39MB
| Movie 2008-07-16 | |
 |
Doc No: IWM013 Document kind: Movie Language: English Size: 1,39MB Expected download time: 3 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: This module shows how to save the station files from a MicroFLO meter (R: memory) that has just been setup to the PC. Then these files are downloaded to the S: memory.
|
 | English - 2,38MB
| Movie 2008-07-16 | |
 |
Doc No: IWM012 Document kind: Movie Language: English Size: 2,38MB Expected download time: 5 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: This module shows the typical changes made to a new MicroFLO meter that should be made to calculate flow at a specific installed location.
|
 | English - 2,53MB
| Movie 2008-07-16 | |
 |
Doc No: IWM014 Document kind: Movie Language: English Size: 2,53MB Expected download time: 6 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: This module shows how to set up the XFC for the host on modbus communications. There is a modbus request block in this module.
|
 | English - 0,00MB
| Movie 2008-07-14 | |
 |
Doc No: Video001 Document kind: Movie Language: English Size: 0,00MB Expected download time: 0 seconds (speed: 56Kb) Published: 2008-07-14 Revision: A File type: txt Summary: Modbus Mapping on NGC 8206
|
 | English - 1,93MB
| Movie 2008-07-16 | |
 |
Doc No: IWM015 Document kind: Movie Language: English Size: 1,93MB Expected download time: 4 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: This module shows how to setup the XFC for the slave on modbus communications. There is an example of mapping registers in the XFC.
|
 | English - 4,15MB
| Movie 2007-02-01 | |
 |
Doc No: WMP002 Document kind: Movie Language: English Size: 4,15MB Expected download time: 10 minutes (speed: 56Kb) Published: 2007-02-01 Revision: A File type: wmv Summary: Activesync is software provided in Totalflow's PCCU NGC installation CD that is used to interface the NGC8206 with the customer's PC via USB cable. This module describes common issues and solutions with activesync/NGC connectivity.
|
 | English - 0,56MB
| Movie 2008-07-16 | |
 |
Doc No: IWM/007 Document kind: Movie Language: English Size: 0,56MB Expected download time: 1 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: Begins with description of AO modules for the XFC and/or the XRC. Then how to calibrate and scale the 4-20 milliamp output.
|
 | English - 0,71MB
| Movie 2005-06-20 | |
 |
Doc No: IWM/005 Document kind: Movie Language: English Size: 0,71MB Expected download time: 1 minutes (speed: 56Kb) Published: 2005-06-20 Revision: A File type: vcm Summary: This module discusses setting up a trend for the battery voltage and the charger. There is information about the register addresses, trend setup, saving the setup, and sending the files to the XFC.
|
 | English - 3,79MB
| Movie 2008-07-16 | |
 |
Doc No: IWM011 Document kind: Movie Language: English Size: 3,79MB Expected download time: 9 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: The session adds a tube to an existing meter. We may not want to completely change the station files. (This would delete all flow data). The added tube uses the ABB multivariable XMV for measurement. This shows how to instantiate new apps and how to connect them together.
|
 | English - 0,64MB
| Movie 2008-07-16 | |
 |
Doc No: IWM/008 Document kind: Movie Language: English Size: 0,64MB Expected download time: 1 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: This module shows how to load a new flash to an existing meter. This is just to replace one flash with the same type flash, just a newer one. The new flash uses the same station files as the old flash.
|
 | English - 1,00MB
| Movie 2008-07-16 | |
 |
Doc No: IWM/009 Document kind: Movie Language: English Size: 1,00MB Expected download time: 2 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: Deletes all station files in the S drive and removes files in the R drive. Then the new station files are loaded in the meter.
|
 | English - 1,12MB
| Movie 2008-07-16 | |
 |
Doc No: IWM/010 Document kind: Movie Language: English Size: 1,12MB Expected download time: 2 minutes (speed: 56Kb) Published: 2008-07-16 Revision: A File type: vcm Summary: Shows how to replace a complete meter but use the station files with the files that were used in the original meter. The station files will be downloaded without the old calibration data.
|
| | | |