Archive
2008-09-18 - ABB the Ex-perts release a new analysers with completely flameproof housing that can be used in plants with potentially explosive gas atmospheres of Zone 1 and Zone 2
2008-06-05 - This project highlights how renewable power sources can be integrated into existing grids to help combat climate change. It is estimated that during its 25 year service life the wind farm will supply clean electricity for up to 90,000 households.
2008-02-09 - Power and automation systems for new production line at Visy mill
2008-02-09 - New ARC study predicts continued robust growth in this global market
2008-01-14 - PickMaster 5 contains all the features necessary to create a robust palletising application without the need to do any robot programming.
2007-12-17 - Take the robot by the hand, and with just a few clicks…arrive at a new dimension of robot intelligence for the finishing process
2007-11-05 - ABB is supplying integrated control and safety systems for the FPSO at Vincent oilfield off the Australian coast - as well as a complete electrification solution for the process module of the oilfield's floating production vessel.
2007-10-12 - Wrigley’s in Australia uses robots to lower labour costs and improve flexibility in producing its world-famous chewing gum.
2007-10-12 - It is estimated that the DiCOM® Alternative Waste Technology facility could generate in total, enough renewable energy to provide the annual electricity needs for up to 2,700 homes.
2007-09-04 - ABB substation solutions has been selected for the Boddington Gold Mine Expansion Project which is designed to become the largest gold processing plant in Australia.