Dubai’s Sustainable City gets power from the sun through ABB inverters

2017-05-02 - ABB string inverters deliver power for the residents of Dubai’s first all- electric city

ABB supports Kayseri OSB project with its solar solutions

2017-04-18 - ABB’s PVS800 central inverters energize the largest solar power plant of 51 MWp in Turkey

ABB launches medium-voltage power protection technology in UK and US

2017-03-28 - PCS120 MV UPS for mission critical facilities including data centers

Vietnam, 7-8 March, Asia Channel Partner Summit

2017-03-23 - A hugely successful event in Ho Chi Minh City

ABB expands its modular UPS product offering for data centers in North America

2017-03-06 - 480V UL version of Conceptpower DPA 500, now with an optimized 300kW UPS cabinet, complementing the data center power chain for ABB

ABB PCS6000 is first medium voltage wind turbine converter to receive certification for applications in China

2017-02-28 - ABB’s PCS6000 medium voltage wind turbine converter has received product certification from the China General Certification Center, CGC. The certification confirms compliance with the Chinese full-power converter guideline for wind turbines GB/T 25387-2010 according to the CGC certification rules CGC-R46022:2011.

EVgo and ABB to Deploy Nation’s First High-Power Electric Vehicle Fast Charging Station

2017-02-27 - National leader in fast charging, EVgo, commissions High-Power EV fast charging station for the next generation of electric vehicles

ABB uninterruptible power supplies: Light industrial UPS versus commercial UPS

2017-02-27 - [No lead text]

ABB to charge the largest single network of 101 electric buses in Europe

2017-02-13 - ABB to charge 101 electric hybrid buses in Belgium using open industry standard OppCharge

ABB brings electric hybrid bus charging to Luxembourg City

2017-02-13 - ABB has installed two fast-chargers for electric hybrid buses at Luxembourg City’s central station. The chargers are based on OppCharge, an open interface for the automated charging of electric buses from any manufacturer, and use a pantograph on the infrastructure to connect the bus to the charging point.

Archive selection