ABB Turbocharging is the world’s leader in turbocharging diesel- and gas engines in the 500 kW plus power range.
24 hours on call at over 90 service stations around the world.
The ABB range of turbochargers has a model for every two- or four-stroke diesel engine designed to operate within 500 to 25,000 kW power range.
ABB Turbocharging has released the A140-H for high-speed diesel andgas engines as the first of its all-new A100 generation.
The new compact turbocharger for medium- and high-speedengines rated 400 kW to 750 kW.
ABB Turbocharging introduces the all-new A100 turbocharger generation as a significant step in the development of single-stage, high-efficiency, high-pressure turbocharging.