It's 6 AM on a construction site and a modular apartment building is taking shape – walls arriving pre-finished, bathrooms pre-assembled, entire rooms lifted into place by crane. The structure that would have taken 18 months to build traditionally is on track to finish in under a year.
 

But there's a problem. Inside those beautiful prefabricated modules, electricians are still doing things the old way: pulling cables, making connections, programming systems unit by unit. The bottleneck that's slowing everything down? The electrical installation.
 

This is the gap that brought ABB and Wieland Electric together.

WHEN TWO WORLDS MEET

Wieland Electric has spent over a century perfecting one thing: pluggable electrical connections. Founded in 1910 and headquartered in Bamberg, Germany, the company has become the world market leader for pluggable installations in functional buildings, with presence in over 70 countries. Their PREFAB® system dominates in factories, logistics centers – places where downtime costs money and reliability matters.

 

ABB Electrification brings something different: decades of expertise in building intelligence. Smart home systems, energy management, building automation, electrical distribution – technology that makes buildings safer, smarter and more sustainable.

 

Separately, both companies were asking the same question: if modular construction can prefabricate entire rooms, why are we still wiring electrical systems on-site? The technology existed. The expertise existed. What was missing was bringing them together.

 

When ABB and Wieland unveiled their collaboration at BAU 2025 in Munich, they weren't just combining product catalogs. They were creating a complete electrical system designed specifically for how modular buildings are actually built by merging ABB's smart building technology with Wieland's pluggable infrastructure into one seamless, plug-and-play solution.

Here's what changes with ABB and Wieland PREFAB:

In the factory, complete electrical systems are assembled, configured, and tested. ABB's smart home devices, energy management systems, and distribution technology are integrated with Wieland's pluggable infrastructure. Everything is pre-programmed. Everything is tested. Digital planning tools ensure every unit is identical.

On site, there are no wire cutters. No programming laptops. Just connections that click into place.

One module arrives. The electrical system plugs in. It works. Move to the next one.

Installation time: up to 70% faster than traditional methods.

REAL-WORLD IMPACT FOR YOUR PROJECTS

  • For project developers and housing associations: Timelines become predictable. A 100-unit apartment building that would take 18 months can be completed in 6-12 months. Costs stop creeping up because prefabrication eliminates on-site surprises.
  • For installers: Repetitive wiring disappears. Skilled electricians spend their time on system integration and consulting—higher-value work that's more interesting and more profitable. The same team can handle twice as many projects.
  • For planners: Clear interfaces. Reproducible standards. No more reinventing the wheel for every identical unit.
  • For building operators: Maintenance becomes straightforward. Systems are documented. Retrofitting is simple. Energy management actually works because it was designed in from the start.
  • And there's an electrical safety benefit too: modules are built in climate-controlled factory conditions, not on scaffolding in February rain.

THE STATISTICS TELL PART OF THE STORY:

6-12 months faster completion

<p>&nbsp; &nbsp;</p>

Up to 70% reduction in on-site installation time

<p>&nbsp; &nbsp;</p>

20-35% material savings

<p>&nbsp; &nbsp;&nbsp;</p>

30% lower installation costs

<p>&nbsp; &nbsp;</p>

Significantly fewer errors

<p>&nbsp;&nbsp;</p>

But the real impact is harder to quantify. It's the installation company that can suddenly compete for projects they couldn't touch before. The developer who can promise (and actually deliver) move-in dates. The electrician who goes home at 5 PM instead of 9 PM because the work is manageable.

THE BIGGER PICTURE

This partnership, unveiled at BAU 2025 in Munich, is doing something unusual: it's making modular construction truly modular, all the way down to the electrical system.

Wireless solutions, pluggable systems, pre-wired distribution boards, and smart home technology are moving from high-end projects into standard residential construction.

 

Behind that simple click (the sound of a Wieland connector locking into place) is a new way of building. Factory precision meets on-site speed. Technology meets craftsmanship. Two industry leaders meet to solve a problem neither could solve alone.

FEELING INSPIRED?

DON’T MISS THE NEXT EDITION!

 

Subscribe and receive the next edition directly to your inbox.