ABB SYNCHRONOUS CONDENSER PACKAGE SOLUTION

To get your data center to market fast, you need to secure stable power even faster. You’ll operate at full speed, even under demanding AI workloads, with the ABB Synchronous Condenser Package. 

 

It's a pre-engineered solution designed to stabilize the interface between data centers, on-site generation, and the grid.

DESIGNING POWER STABILITY FOR AI DATA CENTERS

AI-driven data centers require more than just power capacity - they require system-level stability.

 

In this eBook, you can explore the key stability challenges behind AI workloads, how synchronous condenser solution strengthens your power system, and how they work alongside battery storage to enable reliable and scalable operations.

THE BENEFITS OF SYNCHRONOUS CONDENSER PACKAGE SOLUTION

Get to market with ease and scale designs faster

<ul> <li><p>Reduce on-site construction time with a pre-engineered, modular package</p> </li> <li><p>Implement your power strategy easily with a simpler, scalable and fast-to-deploy solution</p> </li> </ul>

Operate reliably even under dynamic AI workloads

<ul> <li>Protect infrastructure from power fluctuations, reducing risk of downtime and hardware damage</li> <li>Support the continuous, high-load operations required for AI workloads</li> </ul>

Benefit from decades of expertise

<ul> <li>Discuss technical and site requirements with a partner backed by decades of experience in grid stability and power systems engineering</li> <li>Tackle local and global challenges, thanks to our global footprint and experience with complex energy infrastructures</li> </ul>

ASK US ANYTHING
ABOUT GRID STABILITY

If you’re planning a data center project and want to be certain of power stability, our experts are here to help.

FREQUENTLY ASKED QUESTIONS ABOUT SYNCHRONOUS CONDENSER PACKAGE

  1. What is a synchronous condenser?

    Synchronous condenser is a rotating electrical machine that supports the stable operation of electrical power systems. It helps maintain voltage and frequency stability by providing reactive power, physical inertia and short-circuit strength. Unlike a generator, it does not generate continuous active power, and unlike a motor, it does not drive a mechanical load. Its primary purpose is to improve grid stability and power system reliability.

  2. What is a synchronous condenser package for AI data centers?

    Synchronous condenser package is a pre-engineered solution that stabilizes the grid at the interfaces between the utility grid and/or on-site generation and the data center. It provides physical inertia, dynamic reactive power support to maintain stable operation during rapid AI-driven load changes. The ABB Synchronous Condenser Package combines the synchronous condenser, flywheel with integrated safety cage, starting motor with support frame, lube-oil system, eHouse, configurable cooling options (direct, air and water cooling) and optional noise enclosure, into one integrated solution, helping accelerate deployment while ensuring reliable operation.

  3. Why do AI data centers need synchronous condensers?

    AI workloads create rapid and unpredictable power fluctuations that traditional power systems were not designed to handle. These dynamic load changes can impact voltage stability, frequency stability and overall grid reliability. A synchronous condenser provides instantaneous physical inertia, reactive power and fault current contribution, helping protect critical infrastructure while maintaining stable operation under demanding AI workloads.

  4. Can a synchronous condenser work together with battery energy storage systems (BESS)?

    Yes. Synchronous condensers and Battery Energy Storage Systems (BESS) complement each other. BESS delivers fast active power response, while synchronous condensers deliver instantaneous physical inertia, dynamic reactive power for voltage support and short-circuit strength. Together they create a more resilient power system that supports reliable AI data center operation and helps meet evolving grid requirements.

  5. How does a pre-engineered synchronous condenser package reduce data center deployment time?

    A pre-engineered package reduces engineering effort and on-site installation by delivering mechanical, electrical and control systems as one integrated solution. Factory-tested components, design adjusted to the site requirements and single-source delivery simplify project execution, reduce construction complexity and accelerate commissioning, helping data center developers bring new capacity online faster.

  6. How do synchronous condensers support island-mode and microgrid data centers?

    Synchronous condensers help maintain stable voltage, frequency and fault current in island-mode and microgrid-powered data centers. By providing physical inertia and dynamic reactive power, they improve system resilience during rapid AI load changes and support reliable operation. whether the facility operates independently or alongside the main electrical grid.

WATCH THE WEBINAR

Register for our upcoming expert webinar: Power system stability for data centers: Managing dynamic loads while ensuring reliable operation.

 

During the session, you will learn to:

  • understand the evolving power demands of data centers: Gain insight into how digitalization, AI workloads and hyperscale infrastructure are driving rapid growth in electricity demand and changing power consumption patterns.
  • identify emerging power system stability challenges: Learn how renewable integration, converter-based grids and dynamic AI-driven loads are creating new stability risks for data center operations.
  • explore technologies that support reliable and resilient data center power systems: Discover how solutions such as pre-engineered synchronous condensers solution, motors, and generators help maintain stable voltage and frequency in dynamic environments.

LEARN MORE ABOUT GRID STABILITY

Learn more about grid stability

What is grid stability - and why you should care?

Read the article

How ABB helps make renewable grids reliable

Read the article

Stabilizing the future with synchronous condenser

Download the whitepaper

Supporting electrification of Azerbaijan facility

Read the success story