MATERIAL COMPLIANCE

How ABB ensures its use of materials does not endanger vulnerable societies or habitats.

ABB has a duty to ensure that the materials we use do not contribute to environmental degradation. In practice, this means that we have systems in place to monitor and phase out the use of hazardous substances in ABB products and processes, where technically and economically feasible. We have developed lists of prohibited and restricted substances to guide this process and we update them regularly, in line with international regulations.

 

ABB expects suppliers to actively support ongoing efforts to manage and demonstrate product compliance with regulations such as REACH, RoHS, POPs, TSCA, WEEE, WFD, and the EU Battery directive (see below for further information on these regulations). We  require our suppliers and sub-contractors to adopt similar standards and to comply with regulatory requirements.

The ABB List of Prohibited and Restricted Substances has been compiled in order to help our engineers and suppliers comply with regulatory requirements, ensure a high level of protection for human health and the environment, and manage risks encountered by chemicals present in various products.
 

The Guide for Suppliers to the ABB List of Prohibited and Restricted Substances is provided with the purpose of supporting the interpretation of the ABB List and providing guidance on supplier’s obligations.
 

To obtain an older version of the ABB List of Prohibited and Restricted Substances, please contact sustainability.abbzh@ch.abb.com

The European Union Regulation on Registration, Evaluation, Authorization and Restriction of Chemicals (REACH) entered into force on  June 1, 2007. The purpose of this regulation is to ensure high level protection of human health and the environment. This regulation enhances the industry’s responsibility to manage the risks from chemicals and to provide safety information on the substances present in various products. To ensure safe handling, manufacturers and importers are required to gather and disclose information regarding the properties of chemical substances.
 

Legislation similar to EU REACH has been developed in several countries, like e.g., China and South America countries.
 

European Commission - REACH

European Chemicals Agency (ECHA)

China REACH – New Chemicals Registration

The Waste Framework Directive sets out measures addressing the adverse impacts of the generation and management of waste on the environment and human health, and for improving efficient use of resources which are crucial for the transition to a circular economy.
 

As part of the implementation of the EU’s action plan for the circular economy adopted in 2015, the revised Waste Framework Directive entered into force in July 2018. It gave ECHA the task to develop a database with information on articles containing substances of very high concern (SVHCs) on the Candidate List: the SCIP database (Substances of Concern In Products)
 

The SCIP database has three main objectives:
 

  1. Decrease the generation of waste containing hazardous substances by supporting the substitution of substances of concern in articles placed on the EU market.
  2. Make information available to further improve waste treatment operations.
  3. Allow authorities to monitor the use of substances of concern in articles and initiate appropriate actions over the whole lifecycle of articles, including at their waste stage.
     

The SCIP database complements the existing communication and notification obligations for Candidate List substances in articles under REACH.

European Commission – WFD

The purpose of the European Union Directive on the Restriction of the use of certain Hazardous Substances in electrical and electronic equipment (RoHS) is to restrict the use of hazardous substances in electrical and electronic equipment.
 

Legislation similar to EU RoHS has been developed in several countries, like e.g., China, KSA, South Korea, ...
 

European Commission – RoHS Directive
 

China RoHS - EU versus China

In order to assist developing country Parties and Parties with economies in transition in meeting their obligations under the Stockholm Convention, the POPs-free program was initiated in 2010 to facilitate work on the identification of POPs-free products and the exchange of information on alternatives and substitutes to POPs. The program also seeks to involve industry into the implementation of the Convention and to reduce the use of exemptions.
 

Persistent Organic Pollutants (POPs) are organic chemical substances, that is, they are carbon-based. They possess a particular combination of physical and chemical properties such that, once released into the environment, they:
 

  1. remain intact for exceptionally long periods of time (many years);
  2. become widely distributed throughout the environment as a result of natural processes involving soil, water and, most notably, air;
  3. accumulate in the living organisms including humans, and are found at higher concentrations at higher levels in the food chain; and
  4. are toxic to both humans and wildlife

The amount of waste electrical and electronic equipment (widely known as WEEE or e-waste) generated every year in the EU is increasing rapidly. It is now one of the fastest growing waste streams. EU rules on WEEE aim to contribute to sustainable production and consumption.
 

They address environmental and other issues caused by the growing number of discarded electronics in the EU.
 

European Commission - WEEE Directive

The Directive on batteries and accumulators, known as the Battery Directive, is the current text in force regarding the manufacture and disposal of batteries in the European Union. Last amended in 2018, it aims at improving the protection, preservation and quality of the environment. 
 

The Directive mainly covers batteries containing hazardous elements such as mercury, cadmium or lead which, when incinerated or landfilled, present a risk to the environment and human health. It sets maximum quantities for certain types of metals and chemicals contained in batteries, and sets targets for waste battery collection rates, as well as financial liability for waste collection and management. 
 

European Commission - Battery Directive

The PFAS consultation period was planned by the European Commission in September 2023. The commission carries out risk- and socio economic assessments, which are ongoing in 2024. In accordance to the current timeline, first restrictions will become effective in 2027.
 

ABB participated in the PFAS consultation period, and verified the presence of PFAS in products.
 

European Commission – PFAS

Proposition 65, officially known as the Safe Drinking Water and Toxic Enforcement Act of 1986, was enacted as a ballot initiative in November 1986. The proposition protects the state's drinking water sources from being contaminated with chemicals known to cause cancer, birth defects or other reproductive harm, and requires businesses to inform Californians about exposures to such chemicals. Proposition 65 requires the state to maintain and update a list of chemicals known to the state to cause cancer or reproductive toxicity
 

Questions about CA Proposition 65.

The Toxic Substances Control Act (TSCA) Chemical Substance Inventory contains all existing chemical substances manufactured, processed, or imported in the United States that do not qualify for an exemption or exclusion under TSCA. 
 

This may be your starting place for interaction with EPA on TSCA regulatory matters.

Per- and polyfluoroalkyl substances (PFAS) are a large class of thousands of synthetic chemicals that are used throughout society. However, they are increasingly detected as environmental pollutants and some are linked to negative effects on human health.

Your starting place for interaction with EPA on TSCA regulation for PFAS



QUICK LINKS

ABB Supplier Code of Conduct

ABB General Terms and Conditions

Responsible Minerals

ABB Sustainable Supply Base Management Program

GDPR for Suppliers

ABB Supplier Cyber Security