Genix APM Copilot transforms asset performance with AI
ABB has expanded the generative AI capabilities of its Genix Asset Performance Management (APM) solution. The new component – Genix APM Copilot – offers intuitive functionality and streamlined contextualized data flow across processes and operations.
news
3min
2025-09-26
Asset optimization is a key factor in raising productivity
Over the past few decades, many industrial operations have attained levels of sophistication and complexity previously unseen. A desire for high efficiency and low environmental impact, coupled with technology advances and automation initiatives such as Industry 4.0, are just some of the factors driving this transformation of industrial landscapes.
This dramatic change has resulted in an exponential increase in both the number of assets employed in a typical industry setup and their criticality, making the effective management of assets and their performance a crucial task.
APM is a data-driven approach that optimizes the reliability, efficiency and lifespan of physical assets such as turbines, compressors, electrical breakers and instrumentation. The methodology combines predictive analytics, condition monitoring and maintenance strategies to prevent failures, reduce downtime and improve operational performance. APM is crucial for industrial operations such as oil & gas, chemicals, power and water, where asset failures can lead to costly business disruptions and potential safety and environmental risks.
The power of generative AI and LLMs in APM
Efficiency, effective resource allocation and optimized strategic planning have always been at the heart of APM, but the power of generative AI and large language models (LLMs) is making these goals easier to achieve than ever before. ABB, a global leader in industrial automation, electrification and robotics, has teamed up with Microsoft to bring AI-driven intelligence into asset maintenance. Integrating AI into ABB Ability™ Genix has resulted in a new component: Genix APM Copilot, a powerful asset performance and predictive insights assistant, designed to help industries optimize operations and enhance decision-making.
Genix APM Copilot unlocks new levels of efficiency, predictive maintenance and operational insight – leading to safer, smarter and more sustainable industrial performance.
With AI revolutionizing the way industries across the board manage their assets, ABB and Microsoft have positioned themselves at the forefront of this transformation, setting new benchmarks for the future of industrial operations.
AI can support asset management
Genix APM Copilot: flexible AI-powered intelligence for smarter, actionable asset management
Built on the Genix CoPilot foundation, ABB’s scalable and context-aware AI framework, Genix APM Copilot, successfully weaves generative AI into industrial workflows. Unlike traditional AI tools tied to a single provider, Genix APM Copilot is LLM-agnostic − ie, it can work with multiple generative AI models, not just Mirosoft’s OpenAI, which means organizations arenot locked into any single platform or ecosystem.
Genix APM Copilot is also designed for flexible deployment. It can run on cloud, hybrid, or on-premises edge environments, adapting to different IT/OT strategies while ensuring enterprise-grade security and smooth integration with existing IT and OT systems.
In contrast to conventional AI chatbots that merely respond to queries, Genix APM Copilot actively connects with third-party solutions to enable integrated, guided workflows, helping industries proactively manage assets, reduce downtime and maximize operational performance.
Visualization preview of asset performance diagnostics in APM CoPilot.
Instant insights
Generative AI is transforming industrial digital solutions, driving efficiency, intelligence and innovation at an unprecedented pace. ABB’s Genix APM Copilot, powered by multiple LLMs, delivers context-aware insights, generates text, visualizations, and recommendations, and accelerates root-cause investigations with human-machine collaboration, empowering industries to make faster, data-driven decisions with confidence.
By reducing the effort and resources needed to obtain insights, APM users can quickly access answers and act on them within the same workflow, eliminating inefficiencies and improving operational agility. With seamless Genix CoPilot integration, industries can unlock automation of complex tasks, predictive maintenance and in-depth asset analysis, leading to optimized performance, increased asset reliability and reduced environmental impact.
KEY FEATURES AND BENEFITS OF GENIX APM COPILOT
Genix APM Copilot is redefining how industries monitor, manage and maintain their assets.
Natural language interface
Enables chatbot-driven interaction, allowing users to retrieve data, issue commands and execute tasks using conversational AI, eliminating complex navigation. Engineers can ask questions such as, "What failure mode is responsible for the sudden pressure drop in Pump #3?" and receive real-time, contextualized responses.AI-assisted event management
Automates event categorization and prioritization, ensuring engineers focus on the most critical maintenance tasks while reducing fatigue and improving response times.Predictive diagnostics
Leverages analytical AI, physics-based models and sensor data analytics to deliver predictions on equipment performance, diagnosing failures early and preventing unplanned downtime, while generative AI refines these insights via a conversational interface.Enhanced cognitive support
Provides AI-enhanced data analysis, identifying hidden patterns and assisting in analytical tasks, enabling engineers to focus on high-value decision-making.AI-driven deep insights
Combines analytical AI for deterministic predictions with generative AI to contextualize findings, uncover hidden trends and detect anomalies, enhancing reliability and asset performance.Assisted workflow execution
Empowers users to generate maintenance work orders and trigger corrective actions within their APM environment, streamlining operations and ensuring faster, more efficient problem resolution.Having the data at your fingertips is key to informed decisons.
Case studies and potential outcomes
By embedding Genix Copilot capabilities within ABB’s industrial digital solutions, customers can see an up to 30 percent cost savings in operations and maintenance, boost production efficiency by 30 percent and drive up to a 20 percent improvement in sustainability in energy use and emission reduction. The introduction of the generative AI capabilities of Genix APM Copilot is expected to further amplify these benefits, ushering customers into a new era of AI-driven decision-making.
Impact on industrial operations
The integration of generative AI in ABB’s Genix APM Copilot is transforming industrial operations, boosting efficiency, asset reliability and sustainability. Enhanced data collection and faster remediation drive productivity, safety and energy efficiency, while real-time insights empower engineers and executives to act swiftly, reducing downtime and extending asset lifespan.
ABB’s Genix APM Copilot, powered by generative AI, represents a significant milestone in the evolution of industrial digital solutions. By integrating cutting-edge AI technology with ABB's extensive domain expertise, this collaboration with Microsoft is set to revolutionize asset performance management, driving efficiency, sustainability and operational excellence across the industrial landscape.
Sources:
ABB and Microsoft collaborate to bring generative AI to industrial applications
STAY AHEAD IN INNOVATION & TECHNOLOGY
Get our latest news, insights, and breakthroughs straight to your inbox.