Metallurgy’s closest alloy
From the humble paperclip to the majestic Eiffel Tower, metals have shaped our world in more ways than most of us imagine.
news
3min
2025-04-22
Metals have many applications
Industry today uses many different metals and alloys, each having its particular applications. Each metal has its own manufacturing process, involving numerous steps from raw material to finished product. ABB supports metals manufacturers with numerous products and services, from arc furnaces and rolling mills to control systems and sensors.
ARC FURNACES
Arc furnaces require huge amounts of energy
Whether extracting metals from ores in smelting, or melting down scrap metal in recycling, the manufacture of metals typically requires intense heating (and also stirring). Arc furnaces accomplish this with powerful electromagnetic fields that induce large amounts of energy into the charge (as the material in the furnace is called).
With this process being power-hungry, there is a clear case for reducing the energy footprint, savings both costs and emissions. ABB supports this by helping manufacturers optimize the process to reduce energy waste, ensuring just the right amount of energy is applied. ABB’s unique ArcSave technology can reduce energy expenditure in arc furnaces for steelmaking by 3 to 5 percent while lifting productivity by 5 to 7 percent.
ABB's technology
ArcSave®
Electromagnetic stirring for electric arc furnace operation
Whether you work with stainless or carbon steel, you can benefit from significant savings with ArcSave®
ABB Review 3/2016
"A stirring history"
Sustained innovation sums up the history of ABB’s electromagnetic products
ROLLING INNOVATION
A hot-rolling mill
Whereas some metal items can be cast directly in the foundry, many others need further processing. Typically this is performed in a rolling mill. Such a mill uses rolls to flatten slabs into sheet metal (or form into girders, pipes or other shapes). Multiple passes through the rolls are required, with the metal being pressed to very precise thickness and with great homogeneity. The rolling process can furthermore impart other physical properties to the metal such as strength and flexibility.
In steel manufacturing, hot rolling is differentiated from cold rolling, with the resulting steel having different properties.
Rolling mills must not only apply huge pressures but must do so with high accuracy. Motors are used to move slabs in a demanding environment, accurately and efficiently, at the required speed and under varying load conditions.
The South Korean steelmaker, POSCO, recently upgraded a hot strip mill by replacing legacy DC motors with state-of-the-art AC motors and drives packages from ABB. The scope of delivery included 70 roller-table motors. The new motors are expected to deliver considerable savings through greater reliability and lower maintenance needs.
The ACS880 industrial drivers promise further energy savings through greater efficiency, while enabling precise control.
Customer success story
POSCO steel plant
Leading steelmaker POSCO has upgraded a hot strip mill in South Korea by replacing legacy DC roller table motors with state-of-the-art AC motor and drive packages from ABB.
MOTORS MATTER
A highly efficient IE5 SynRM motor
Metals manufacturer, Aurubis, is implementing a major upgrade at a copper plant in Bulgaria. It is replacing 460 older, inefficient motors by highly efficient IE4 and IE5 motors. Many of these will be paired with matching ABB drives. The upgrade will save so much energy that the project will pay for itself in only 3.5 years. Other benefits include reduced energy consumption by 28 percent and carbon emissions by 12,000 tons annually, increased process flexibility and improved performance.
Customer success story
Aurubis - copper producer
Aurubis is implementing a major upgrade at its copper plant in Bulgaria, with 460 older, inefficient motors replaced by IE4 & IE5 motors. Many of these will be paired with matching ABB drives. The upgrade will save so much energy that the project will pay for itself in only 3.5 years.
ENGINEERED TO OUTRUN
These are just a small selection of the products and services ABB provides to the metals industries. With its deep knowledge and experience, ABB is poised to help metals industry outrun, leaner and clear.
STAY AHEAD IN INNOVATION & TECHNOLOGY
Get our latest news, insights, and breakthroughs straight to your inbox.