ABB pumps up water sustainability with smart technologies

Few resources are as vital to our health and well-being as clean water and sanitation. What we easily take for granted would not be possible without myriad sophisticated technologies – to be found from water extraction and purification plants, through pumping and delivery, to the efficient removal of wastewater and its processing.

news

2min

2025-03-19

An aerial view of a city skyline with a lake, industrial facilities, and circular water treatment tanks surrounded by greenery.

 

ABB supplies many of the components and technologies of our water and waste-water networks, including grid connections and protection, drivetrains for pumps and monitoring and control systems.

 

In many parts of the world, water is a scarce resource. Even where this is not the case, energy must typically be expended in purifying and pumping it, meaning every drop of water wasted also involves energy being wasted. Detecting and repairing leakages is vital to upholding and improving the sustainability of our water supply. Measuring the lowest flows is essential in addressing one of the biggest challenges facing the industry - detecting leaks when they are small. Monitoring systems quantify flows within a water network, and help localize leakages, permitting a more time-consuming and cost-effective deployment of repair crews. Monitoring also helps understand usage patterns and thus better plan operations and future investment.

 

With flow measurement being vital to the health of water networks, the flowmeters themselves must be as reliable and as possible, requiring minimal repairs or inspections.

 

USING FARADAY’S LAW FOR FLOWMETERS

The key to reliability is the absence of moving parts. Furthermore, a flowmeter should not obstruct the flow of the water, and its own power consumption should be low. This is just the job for an electromagnetic flowmeter. A flowmeter uses Faraday’s law of electromagnetic induction to quantify the flow of liquid.  As part of the process, the (conductive) liquid flows through a magnetic field, and induces a voltage in the same way that a dynamo would. This voltage can be measured, and the flow rate calculated from it.  One example of an electromagnetic flowmeter application is in the Yanbu desalination project in Saudi Arabia, designed to provide drinking water to 1.5 million people in the city of Medina and surrounding areas. The installation will feature super-sized flowmeters with an inside diameter of three meters).

Efficiently powering the pumps

Another important ABB contribution to water networks is efficiently powering the pumps.  With every drop of water requiring energy to pump, the electric motors and drives that power the pumps need to be as energy efficient as possible, while also providing high reliability, often under harsh conditions such as moist and corrosive atmospheres and extreme climatic conditions.

 

Many legacy water networks run their pumps at a fixed speed. They use variable throttles to slow the water to the desired flow. This is a waste of energy. A variable-speed drive (VSD) controls the motor to the precise speed and torque required, while also providing monitoring functions with precise information on the flow and on their own operation. Such VSDs are designed to be easy to install and configure, and offer functionalities specifically tailored to pumping operations.


ABB also offers matching motors, designed for robust operation with minimal maintenance, providing the highest level of efficiency. They have IP55 protection for use in dirty and wet environments, while upholding high energy efficiency.

Read more

ABB offers a range of efficient water solutions to control and optimize the pumping of clean water.

ENGINEERED TO OUTRUN

Next time you open a tap, give a thought to the technologies that made that glass of cool, clear, nourishing water possible. This is but one example of the many ways in which ABB helps water industries outrun - leaner and cleaner.

STAY AHEAD IN INNOVATION & TECHNOLOGY

Get our latest news, insights, and breakthroughs straight to your inbox.