People power

A conversation with Veli-Pekka Peljo, who led the multidisciplinary team that created ABB Dynafin™.

news

3min

2024-08-18

Veli-Pekka Peljo, Senior Project Manager, Solutions Development →01, joined ABB Marine & Ports in 2003 as a design engineer and immediately rolled up his sleeves on the continued development of ABB’s Azipod® propulsion technology. Ten years later, he was called on to helm the multidisciplinary team that gave birth to ABB Dynafin, launched in May 2023. Here, he explains how the concept came into being, the collaborative effort needed to bring it to the prototype stage and why a clear goal and open mindset are key to handling uncertainty.

 

It has been a long journey since 2013, when Peljo took charge of ABB’s Total New Propulsion project to develop a propulsion unit with an efficiency of over 80 percent. “Already then, electrification of vessels was seen as a trend, but the green transition was still to come. At that time, marine fuel prices were at an all-time high, so fuel efficiency and reducing emissions were at the front of people’s minds and became the main drivers for the project.” 

01 Veli-Pekka Peljo is passionate about ABB’s work in advanced marine propulsion concepts.

 

Defining moment

 

The resulting prototype was hydrodynamically tested in the VTT model basin in Espoo, Finland and then self-propulsion and maneuvering capabilities were confirmed in open-water lake trials in Sweden. It worked as predicted. “We did everything you’d do in a full-scale sea trial program. That was a fantastic milestone and confirmed all our hard work. We knew then we could really make the concept, which we originally called ‘Foilwheel,’ fly as a world-first digital propeller with extraordinary efficiency,” comments Peljo.

 

To those who might wonder why nobody had done this sooner, Peljo’s answer is: it’s not that simple. “ABB Dynafin may look similar to some mechanical solutions, but inside it’s totally different – the main thing being the blade motors and entire drive train. 

 

Instead of mechanical levers controlled by hydraulic servo actuators, we have electric motors with low RPM and high torque that we can match with the propeller blades at full scale.”

 

He says the final ABB Dynafin units will be of standard design, although of different propeller diameter sizes depending on the power factor. This shortens delivery lead time. “Then you just select the right blade length to fit the vessel draft. It could be that we offer only two different blade lengths, but our target is to keep the blades above the baseline.”

 

The fatigue strength of the blades is a critical design issue, so they need very careful design to ensure the required service life with high reliability. “We’re currently thinking martensitic casted stainless steel but given certain manufacturing constraints, we may need to use composites for the longer blades on higher-power units. We’re also working on details like sealing solutions to achieve an optimal total cost of ownership.”

 

 

Target markets

 

In terms of which vessels the concept is most suited to, Peljo explains that right now they are “just scratching the surface.” He elaborates, “we are aligning it with customer requirements for different segments, but there are a lot of possibilities. Transit vessels will see the biggest benefit and the faster the speed, the bigger the benefit. But we’re mostly looking at 12 to 20 knots at this stage. With ABB Dynafin, you get many different design points in just one propeller: one for maximum sea-trial speed, one optimized for economy speed, one for safe return to port at six knots, one for dynamic positioning operation and so on. It’s very versatile and can suit all sorts of ship types.”

 

In terms of power factors, ABB is working towards four sizes, from 1 MW to 4 MW. Four 4 MW units on a vessel would give propulsion power of 16 MW. “There’s interest in the market to go even higher, so we’re also looking at 5 MW units and upwards,” adds Peljo.

 

Thanks to its integrated controllable pitch propeller (CPP) feature, ABB Dynafin has the dynamic positioning capability necessary for offshore vessels. “It can change thrust direction through 180 degrees in seconds, providing a very fast response time if you need to change vessel heading. With multiple units, we’re also looking at how ABB Ability™ Marine Pilot Control can best utilize ABB Dynafin unit’s capabilities for all operational modes and autopilot configurations, with a view to remote operations and eventually autonomous operations.”

 

There are also low-vibration vessel cases. “The RPM is quite low at full power, but the amplitude is higher. The pressure pulses from a vertical propeller don’t interfere too much with the hull, but we can tweak the blade trajectories even more to eliminate vibration and noise almost completely for silent operations.”

 

Moreover, ABB Dynafin boasts other valuable features, such as regenerating power when braking the vessel, just like a self-charging hybrid car. “You can charge onboard batteries simply by the action of the water turning the blades like a windmill. 

 

Then we also have the so-called rudder mode, meaning that, when the propulsion drive is inactive, that is, with the main wheel stopped, all the blades can work together to steer, for example, a sail-assisted vessel →02.”

 

 

Dealing with uncertainty

 

Peljo highlights that there is always uncertainty when developing a new concept from scratch. “To handle that, the human factor has to be constant; it’s essential to maintain a creative, open mindset and a strong focus on the goal even if the requirements are vague. Innovation is not all about luck and in-the-moment inspiration; we had a lot of arduous concept rounds. Looking back, we could, of course, have moved faster, but we’ve had a lot of parallel projects to work on, too,” he adds.

 

Having a proven R&D methodology is also crucial. “We use the applied ship design spiral, where you move from mission requirements to high-level concept analysis on the outer circle and gradually work inwards, honing the design in greater detail. You can’t get bogged down in details too soon. Having a clear business case also stops you from getting distracted in theoretical niceties that waste time.”

 

 

 

Kudos for partners

 

Peljo stresses that there was “no way we could’ve done this alone.” ABB Dynafin has been the result of pulling together expertise in mathematics, hydrodynamics, mechanics, electrical and control, and we’ve had great partners in Aalto University, VTT and the ABB CRC. So, having the right mix of people, combined with ABB’s strong culture of innovation and determination to always do better, has been crucial for success.”

 

As to his personal motivation, Peljo trained as a mechanical engineer and loves R&D work because no one day is the same as another. “I’d be bored stiff doing the same thing day in, day out. The project was a once-in-a-lifetime opportunity and it’s fantastic to have come so far in bringing ABB Dynafin to reality.”

 

“Given the high cost of new green fuels and the increase in fully electric vessels, the business case is even more attractive,” Peljo adds. “Contributing to the green shift gives extra meaning and I believe it’s great timing for what is an exceptional novel technology. We are working hard on the details and I can’t wait to see the first ABB Dynafin live on a real ship.”

02 ABB Dynafin can operate in rudder-only mode for sail-powered vessels or when hybrid vessels switch to sail-assisted mode.

STAY AHEAD IN INNOVATION & TECHNOLOGY

Get our latest news, insights, and breakthroughs straight to your inbox.