Pioneering technology to electrify Japan’s mining industry

Web Story

5min

2025-05-12

A global thirst for raw materials that power the energy transition has led to booming demand¹ for metals and elements to make batteries, motors, drives and other essential electrification components.

ABB and Hitachi Construction Machinery are field-testing this jointly developed electric dump truck

 

Metals including lithium, cobalt, nickel, copper, aluminium and manganese, along with conductive elements such as graphite, are more sought after than ever – a need which is making new demands of the mining sector.

 

Mining is an energy-intensive industry, responsible for up to seven percent of global greenhouse gas emissions². A large volume of these is attributed to diesel-driven vehicle movements in open-pit and underground mines.

 

Japan is home to a number of the world’s leading manufacturers of mining equipment, such as mining trucks, and we are collaborating with companies including Hitachi Construction Machinery, Komatsu and Sumitomo Corporation to help them achieve decarbonization and efficiency goals in this vital industry.

 

TESTING WORLD’S FIRST ULTRA-LARGE ELECTRIC HAUL TRUCK

Since 2021, ABB and Hitachi Construction Machinery have jointly developed the world’s first ultra-large fully electric haul truck. It was shipped to Zambia’s Kansanshi copper-gold mine during 2024, where it has undergone trials over subsequent months.

 

These are the world's first³ technological feasibility trials of an ultra-large full battery haul truck by an OEM (Original Equipment Manufacturer) at a customer’s mining site.

The ABB-Hitachi Construction Machinery electric dump truck under construction

The trials are being conducted to support Hitachi Construction Machinery’s goal of transforming its trucks from diesel to full battery operation, using our high-performance traction battery and highly energy-efficient DC/DC converters.

 

On level ground, the truck runs on its internal battery, then, when moving uphill, its onboard electric system draws energy from a trolley supply to power the motor directly, as well as charging a battery energy storage system.

 

When running downhill, the truck’s regenerative braking system charges the battery, reducing the charging load when the truck is connected to the trolley. This virtuous circle reduces the truck’s overall energy use and enables it to stay in continuous operation with no charging breaks and maintain high productivity.

 

A sophisticated battery energy and thermal management system maximizes service life of the batteries.

Hybrid and fully electric dump trucks are clearly the future, but the transition needs to begin now. Big mining companies have their clear targets to achieve net zero by 2050 and this will not be possible if they don’t electrify the mining truck fleets.

Fabiana Cavalcante, Global Head of Mobile e-power, ABB

PARTNERING WITH KOMATSU TO FIND DECARBONIZATION SOLUTIONS 

 

A further collaboration is designed with Japan’s Komatsu – one of the world’s largest providers of construction and mining machinery – to jointly create electrification and decarbonization solutions, ranging from renewable energy generation to fully electrified mining equipment for customers, through an open platform.

 

Both companies are committed to accelerating decarbonization in mining, and have established a joint team to develop and bring to market integrated solutions that will help reduce diesel consumption and ultimately eliminate it through the electrification of mine operations. ABB’s contribution to the collaboration will be in the areas of automation and electrification.

By working together, we will tackle electrification and make a revolutionary difference to the way mining companies operate their sites in the near future.

Max Luedtke, Global Business Line Manager for Mining, ABB Process Industries

SUMITOMO AND ABB TO EXPLORE DECARBONIZATION OF MINING MACHINERY 

ABB and Sumitomo have agreed to collaborate on research into decarbonizing mining operations

 

Building on our collaboration with Komatsu, we have entered an agreement with Japan’s Sumitomo Corporation, designed to establish strategies and recommendations for technology systems in heavy industrial applications, such as mining.

 

We’re working with Sumitomo’s Construction and Mining Systems Strategic Business Unit, to explore joint solutions for decarbonizing the operations of mining machinery, with a focus on fleet electrification and renewable power integration.

Together with Sumitomo, we’re prepared to make further inroads to the challenge of decarbonizing heavy machinery in the mining industry. As a technology leader we do not take this responsibility lightly and mean to investigate all routes to drive effective change for leaner and cleaner operations. No organization can do this alone, and we share strong values and ideas with our new partner.

Joachim Braun, Division President, ABB Process Industries

ABB EMINE™ AND ALL-ELECTRIC MINING

eMine™ makes the all-electric mine possible, with fully integrated electrification and automation systems from mine to port. From design to ongoing service, ABB is the partner that can transform today’s mine operations while improving the world beyond them.

Sources:


1. IEA: The role of critical minerals in clean energy transitions
2. Climate risk and decarbonization: what every mining CEO needs to know 
3. As of June 27, 2024, based on a survey conducted by Hitachi Construction Machinery of ultra-large dump trucks with a load capacity of 150 tons or more manufactured by OEMs

ABB STORIES HUB

From electrification breakthroughs to automation marvels, explore how ABB is shaping a more sustainable and resource-efficient future.