Powering thrills and roller coaster safety worldwide

When you think of electric motors, amusement parks, skydiving tunnels, and gravity-defying rides may not be the first things that come to mind. However, our advanced motor and drive technology plays a crucial role in delivering unforgettable thrills in some of the most unexpected places. From vintage carousels to extreme skydiving simulators, our drives and motors bring precision, efficiency, and safety to the world of entertainment.

Web Story

5min

2025-06-26

When you think of electric motors, amusement parks, skydiving tunnels, and gravity-defying rides may not be the first things that come to mind. However, our advanced motor and drive technology plays a crucial role in delivering unforgettable thrills in some of the most unexpected places. From vintage carousels to extreme skydiving simulators, our drives and motors bring precision, efficiency, and safety to the world of entertainment. 

 

A HISTORIC CAROUSEL WITH A MODERN TWIST

Carousels have been delighting riders for generations, and our technology is helping to ensure their timeless magic continues. At the Bushnell Park Conservancy Ohio, an iconic, hand-carved wooden carousel has been brought into the modern era with ABB variable frequency drives (VFD). To ensure safe, efficient operation, Bushnell Park partnered with ABB’s Flow Tech, Inc. to replace the aging VFD and motor with an ACH580 drive and a Baldor-Reliance motor with grounding rings. This upgrade from a 480V unit to a 15 hp, 208V ACH580 allows adjustable speeds, making it ideal for young children, seniors, and thrill-seekers alike. It also allows for reducing energy consumption, and the replacement was scheduled during off hours and off season, preventing downtime and revenue loss. Thanks to this reliable solution, the carousel will continue to delight riders for years.

ABB Drives keep Bushnell Park Conservancy's 1914 carousel running smoothly.

A GRAVITY-DEFYING THRILL RIDE IN SWEDEN

For those seeking more adrenaline, our motors are behind one of Sweden’s most exciting amusement park attractions. The Loke Gyro Swing at Liseberg amusement park in Gothenburg uses an ABB industrial drive to replicate some of the physics of space travel, safely and precisely while conserving energy. The innovative attraction at Liseberg amusement park challenges riders with gravity-defying movements, delivering a unique and unpredictable experience. Roller coaster safety is crucial and this ride's motion relies on ABB motors and drives, which provide precise control over acceleration and deceleration, ensuring both excitement and safety.

SMOOTH AND SAFE ON HYPERION

At Energylandia, one of Europe’s leading amusement parks, thrill-seekers can experience Hyperion – the continent’s tallest and fastest roller coaster in its category. After a slow climb to nearly 80 meters, riders plunge at speeds of up to 142 km/h through tunnels, twists, and inversions.

While gravity powers most of the ride, the journey begins with a reliable electric drive system. An ABB variable speed drive ensures a smooth, controlled ascent and a gentle start, delivering the power needed to lift fully loaded trains safely and efficiently. Selected by the roller coaster manufacturer and supported through regular maintenance, ABB technology helps keep Hyperion operating reliably, providing both safety and comfort for millions of visitors seeking an unforgettable experience.

THE SCIENCE BEHIND INDOOR SKYDIVING

For those who dream of flying, Switzerland’s first free-fall simulator in Sion allows for this. At the Realfly simulator, 20,000 guests a year experience this thrill in a safe indoor facility – with a reliable ABB drive.

Our low-voltage motors power massive fans that generate a controlled column of air strong enough to lift people off the ground, allowing them to experience the sensation of freefall—without the need for an airplane. These wind tunnels require extreme reliability and precision, as even the slightest inconsistency in airflow could impact the experience. 

For more than ten years, ABB systems have been powering this closed air circuit, specifically four robust M3BP  electric motors, each with an output of 250 kilowatts. They are supplied by an ACS800 Multidrive frequency converter with exactly the power they need for the desired wind speed.

 

PUSHING THE LIMITS OF HUMAN FLIGHT

Another cutting-edge skydiving simulator, developed by EVG Lufttechnik, takes ABB technology to new heights. This advanced system uses high-performance ABB motors to generate powerful airflow, allowing skydivers to practice manoeuvres in a controlled environment. The challenge? Simulating real-world skydiving conditions with perfect airflow stability. Our motors provide the precision needed for users to experience smooth, uninterrupted flight, while also keeping energy consumption low. Whether training for professional skydiving or simply experiencing the thrill of human flight, ABB motors are at the heart of this exhilarating innovation.

SAFE ACROBATICS IN 300 KM/H AIRFLOW

You don’t need to jump out of an airplane to experience the sensation of freefall. At FlySpot near Wrocław, visitors can simulate a skydive in a state-of-the-art wind tunnel, where airflow reaches speeds of up to 300 km/h.

At the heart of the facility are four ABB electric motors powering fans that move massive volumes of air every second. ABB variable speed drives enable precise and continuous control of airflow, allowing instructors to safely adapt flight conditions for everyone—from first-time flyers to professional athletes. Combined with ABB SafePlus switchgear for reliable power distribution, the technology helps ensure a safe, energy-efficient, and immersive flying experience. Trusted by world champions for training and by beginners seeking adventure, FlySpot demonstrates how ABB solutions bring performance, reliability, and safety together in demanding applications.

POWERING FUN WITH PRECISION AND RELIABILITY

From amusement parks to high-tech skydiving simulators, ABB motors and drives are found in unexpected places- bringing excitement, safety, and efficiency to experiences that millions enjoy worldwide. Whether you're spinning on a vintage ride, defying gravity in Sweden, or flying indoors in Switzerland, ABB is there — powering unforgettable experiences around the world.

READ MORE

Smart & Sustainable Buildings | Circular Construction

Discover how ABB enables smart and sustainable buildings through digitalization, automation, and circular construction—driving energy efficiency and low-carbon cities.

Engineering the Backbone of Modern Aviation - ABB at the Navi Mumbai International Airport

ABB`s technologies at the Navi Mumbai International Airport

Powering and protecting systems in the world`s tallest building

ABB’s technologies play a vital role in powering and protecting the Burj Khalifa since 2010 enabling reliable and efficient operations

Powering thrills and roller coaster safety worldwide

ABB motors and drives power thrilling rides, carousels, and skydiving simulators worldwide—delivering fun with precision, safety, energy efficiency, and reliability.

Shaping the future of sustainable hospitality

Sustainable hospitality integrates smart energy systems and automation. Discover how ABB enables energy-efficient hotels and venues.

Smart stadiums: Running the future of sports venues

Smart stadium automation transforms large venues into energy-efficient, digitally connected spaces. Learn how ABB integrates intelligent building systems to reduce energy use.

Using the earth’s heat to power US data centers and homes

Geothermal energy supports reliable, low-carbon power generation. Learn how ABB enables geothermal integration and grid innovation in the United States.

Investing for success in the United States

ABB's $14bn investment in United States manufacturing in recent years is enhancing digital presence and creating jobs across multiple industries.

Helping CERN save energy as it probes the mysteries of the universe

Energy efficiency at CERN demonstrates how ABB supports large-scale scientific research with advanced, energy-efficient power systems.

The innovative technology powering Saudi industries

How ABB supports the tech behind the tech

Learn how ABB's innovative technology is powering the development of Saudi Arabia's industries, from energy to transportation and beyond.

Keeping pilgrims cool at Makkah Grand Mosque

How does ABB's technology keep Saudi Arabia’s Makkah Grand Mosque cool, ensuring comfort for millions of religious pilgrims?

Shaping the future with efficient, sustainable construction

Future-ready construction combines efficiency, sustainability, and digital innovation. Discover how ABB helps build tomorrow’s infrastructure with advanced building solutions.

Electrifying sustainable tourism in Saudi Arabia

Smart infrastructure enables sustainable tourism at scale. Learn how ABB supports smart cities and energy-efficient tourism development in Saudi Arabia.

Emissions cut at ABB Mexico factory, with Mission to Zero™

Since committing to the Mission to Zero blueprint for sustainable operations, ABB's factory in Saltillo, Mexico has reduced emissions by more than 5,200 tons of CO₂e.

Sustainable manufacturing: Contagem Mission to Zero™ site

The challenge facing ABB’s Belo Horizonte site in Contagem, south-east Brazil, was how to transform a 50-year-old factory into a beacon for sustainability. This is how the workforce set about making it run leaner and cleaner.

The power of calculators - from everyday tasks to business insights

The power of calculators - from everyday tasks to business insights

Calculators play a crucial role in helping customers estimate the potential reductions in carbon dioxide-equivalent emissions enabled by ABB solutions.

Enabling energy-efficient buildings

Buildings are central to the net-zero transition. Explore how ABB technologies enable energy-efficient buildings with lower emissions and smarter energy use.

ABB STORIES HUB

From electrification breakthroughs to automation marvels, explore how ABB is shaping a more sustainable and resource-efficient future.