Shaping the future of sustainable hospitality
Today’s travelers expect more than just comfort and amenities - they’re prioritizing sustainability in the hospitality industry when choosing where to stay.
Web Story
7min
2025-02-24
From concepts like eco-tourism to facilities with EV chargers, sustainability is becoming a key factor in choosing accommodations. The shift reflects a growing awareness of environmental responsibility in the hospitality industry.
Growing demand for green travel
<p><b>75%</b> of global travelers express a desire to travel more sustainably in the next 12 months. Specific intentions include <b>reducing energy consumption (57%),</b> <b>using more sustainable modes of transport (54%)</b> when traveling in the future.<sup>1</sup></p>Economic influence of global tourism
<p>The industry contributes, directly, indirectly and through induced impacts, roughly <b>4% of global GDP</b> (US$4.9 trillion in 2024) and supports around <b>349 million jobs</b> worldwide.<sup>2</sup></p>Carbon footprint of lodging
<p>In 2023, accommodation alone was responsible for about<b> 260 million tonnes of CO<sub>2</sub></b>.<sup>2</sup></p>MORE THAN A TREND - A CRITICAL BUSINESS DECISION
Sustainability in the hospitality industry is more than a trend - it’s a critical business factor. However, the hospitality sector faces a dual challenge: delivering exceptional guest experiences while minimizing its environmental impact. Hotels are among the most resource-intensive operations, requiring significant energy to maintain guest comfort.
For venue operators, the performance of heating, ventilation, and air conditioning (HVAC) systems is critical to both operational expenditure and guest satisfaction. These systems can account for up to 60 percent of a venue's total energy consumption and are therefore prime targets for optimization.
ABB’s technologies address these challenges by empowering hotels and resorts worldwide to run leaner and cleaner, with innovative solutions that help redefine sustainable hospitality through energy efficiency and environmental stewardship.
ENERGY CONSUMPTION, COST, AND GREENHOUSE GAS EMISSION DATA OF HOTEL BUILDINGS [3]
SUSTAINABLE BY DESIGN
ABB building automation solutions are supporting the hospitality industry with digital solutions designed to elevate guest comfort and streamline hotel operations for cost reduction and improved operational performance.
For example, in a hotel, cooling or heating demand can vary throughout the day based on occupancy levels and outdoor temperatures. Variable Speed Drives (VSDs) can regulate the speed of fans and pumps to match the fluctuating demand, ensuring that power is only used when necessary and that HVAC systems do not consume excess energy during times of low demand. This dynamic adjustment can lead to a reduction in energy consumption of 25-40 percent, depending on the system and building design, resulting in significant energy cost savings.
Another example, the worldwide standard for home and building automation, KNX, enables all devices to communicate with one another via a single bus cable, streamlining all electrical functions that are connected for easier management and control. The operational flexibility of an ABB i-bus® KNX electrical installation includes components ranging from lighting, shading, and temperature control to energy management. Installing a KNX system can lead to a reduction in energy consumption from lighting and room heating control by up to 40 percent.4
Recently ABB unveiled GuestFlow, a fully integrated Guest Room Management System (GRMS) developed for hotel owners, operators, and system integrators. GuestFlow integrates presence detection, smart heating, ventilation and air conditioning (HVAC) control, lighting automation, to optimize energy use in real time. This helps reduce operating costs, support sustainability goals, and protect long-term investments.
CASE STUDIES FROM AROUND THE WORLD
<p>Learn how we’re supporting the industry worldwide to run leaner and cleaner</p>
Belgium
Innovation platform Living Tomorrow used ABB’s energy efficient technology in their Brussels campus. The latest digital and automated solutions give guests control over their environment with the touch of a button and building operators increased visibility to energy use and emissions. The campus offers eight state-of-the-art meeting rooms, a hotel with 92 guest rooms, an auditorium, two restaurants and a digital experience center.
Italy
ABB has provided solutions to two leading hotels, both focused on improving sustainability in their operations. At the four-star Le Fucine hotel in Buttrio, we have collaborated with owners, the Danieli Group, to integrate technology that increases both guests’ comfort and the hotel’s energy efficiency. Further south, in Tuscany, the ADLER resort hotel has also turned to ABB to renovate their electrical systems. The ABB Ability™ Energy and Asset Manager platform was implemented to allow real-time energy consumption monitoring.
Spain
At the InterContinental Hotel in Madrid, ABB’s drives and high efficient motors have reduced energy consumption by 40 percent, showcasing how smart building technology can revolutionize sustainability in hospitality.
Finland
The Original Sokos Hotel Royal in Vaasa is being transformed into one of the most energy-efficient hotel in the Sokos chain, without losing its historic charm. Thanks to the ABB i-bus® KNX system, rooms prepare automatically before guests arrive, lighting responds to presence, and energy is used only when needed. Powered by geothermal heat and solar panels, the hotel runs primarily on renewable energy.
The Panorama Landscape Hotel offers guests a luxurious escape with its unique landscape suites, forest spa, and fine dining. Behind its serene ambiance, ABB’s advanced building automation solutions ensure seamless adaptability to guest needs via intuitive touchscreens while optimizing energy efficiency in lighting, heating, and cooling - blending rural luxury with cutting-edge sustainability.
Switzerland
The Dolder Grand pairs its renowned luxury with innovative energy efficiency and power protection, supported by ABB’s uninterruptible power supply (UPS) systems. In the event of power failure, ABB's UPS ensures emergency lighting and systems remain operational while significantly enhancing energy efficiency and saving approximately 13,500 kWh annually.
ABB has also integrated smart building technology into a historic thermal spa, merging wellness traditions with modern energy-efficient solutions. This initiative enhances guest comfort while reducing environmental impact, embodying sustainable hospitality.
Turkey
The ID Bodrum project on Turkey’s scenic Bodrum peninsula integrates ABB’s smart building solutions. With ABB’s i-bus® KNX and Cylon® HVAC automation, the buildings achieve enhanced energy monitoring, reduced utility costs, and seamless automation, combining elevated comfort with sustainable innovation.
Lapland and Greenland
ABB’s advanced KNX building automation technology powers the energy-efficient operation of glass igloos in Lapland and Greenland, ensuring seamless performance even in extreme weather conditions. Residents can easily control lighting, ventilation, and power settings to conserve energy, while hotel staff can remotely manage and adapt systems during vacancies, optimizing efficiency and reducing manual intervention.
India
Amanbagh, a resort nestled in the Aravalli Mountain range of Rajasthan installed more than 50 ABB drives on the air handling units and pumps of the resort’s HVAC system. When compared to the conventional damper or valve control solution, drives can adjust the motor speed of fans or pumps to meet the current building needs, thus smartly saving a lot of energy. This way, the resort was able to save around 30 percent of its energy annually.
Thailand
Located in the heart of Bangkok, the Unicorn Phayathai is designed to provide a multifunctional hub for work, leisure, and mobility. The building uses ABB Ability™ Energy and Asset Manager, ABB Motor Control Center technology and ABB’s Terra electric vehicle charging systems. ABB Ability™ Energy and Asset Manager provides real-time insights to optimize energy consumption and reduce operational costs by up to 40 percent.
Middle East
The Four Seasons in Doha has ambitious sustainability targets and reached out to ABB for support. The upgrade works included the replacement of 20 air circuit breakers with ABB’s Emax 2 smart circuit breakers, retrofitted five Ekip UP retrofit devices and connecting the substation to the ABB AbilityTM Energy & Asset Manager. By improving overall performance, the solution can save up to 20 percent on energy bills; 40 percent on maintenance costs; and 30 percent on operational costs.
The luxury Ashar Tented Resort in AlUla's Ashar Valley has been equipped with our advanced electrification systems, including intelligent lighting control, building automation, and a comprehensive low-voltage power infrastructure anchored by ABB's System pro E Power Main Distribution Switchboard. These technologies ensure uninterrupted power supply and optimized energy flow across the resort's climate control, lighting, and critical functions, enabling seamless operations in the remote desert environment while supporting Saudi Arabia's vision for world-class sustainable hospitality.
<p> </p>
Netherlands
ABB provided a comprehensive electrical and lighting solution for the Van der Valk hotel in Lelystad, Netherlands, helping the 143-room, sixteen-floor property meet its goals of sleek design, safety, and fast construction. Working through installation partner Techval and distributor Rexel, ABB supplied 200 Evago emergency luminaires across escape routes, lobbies, and common areas, along with Aqualux luminaires for the hotel's swimming pool. Wieland plug-and-play connectors allowed the full emergency lighting installation to be completed in just eight months.With a lifespan of up to 12 years and a modular design that simplifies repairs, the system is built for the long term. ABB's i-bus® KNX controls and energy management system are already planned for further rollout across additional Van der Valk locations.
Brazil
On the coast of Santa Catarina, Brazil, Felissimo Exclusive Hotel has set a new benchmark for sustainable luxury hospitality. Within the hotel, the Casa Verde suite is fully equipped with smart building solutions from ABB Electrification, including KNX-based automation, solar energy integration, and electric vehicle (EV) charging infrastructure. Estimates based on technical standards and usage patterns at the hotel suggest that Casa Verde uses 20 percent less electricity than a comparable suite without automation.
Sweden
The newly opened Hernö Gin Hotell on Sweden's High Coast used our Impressivo switch series throughout its 122 luxury rooms. The Impressivo switch series, manufactured at our Mission to Zero factory in Helsinki, features PVC- and halogen-free construction that eliminates harmful chemicals from the hotel's rooms. The project's sustainability was further enhanced through innovative project packaging that minimized transport requirements and material waste—delivering pre-packed room kits reduced both installation time and environmental impact.
South Korea
To support MONA YONGPYONG’S ambition of becoming a year-round, sustainable luxury residential development, ABB delivered a comprehensive KNX-based smart building infrastructure. With more than 600 ABB Trevion® Keypads and Trevion® displays installed, the system enables intelligent, scalable control that’s tailored to the evolving needs of residents. Implemented in collaboration with Kaiser Solution, the system integrator supplying ABB products and ensuring seamless integration.
Footnotes
- Booking.com’s 2024 Sustainable Travel Report
- Towards circular hospitality - Circle Economy, Iberostar Hotels & Resorts & UN Tourism White Paper
- Toward Sustainability: Interventions for Implementing Energy-Efficient Systems into Hotel Buildings
- Elevating Luxury Ambience with KNX Building Automation at Panorama Landscape Hotel in Finland's Tahko Hills
SHAPING THE FUTURE OF SUSTAINABILITY IN THE HOSPITALITY INDUSTRY
With innovative solutions helping the hospitality industry reduce its carbon footprint, and achieve operational efficiency without compromise, ABB enables the hospitality industry to outrun leaner and cleaner.