Sustainability in motion: what lifecycle assessments reveal about modern aluminium manufacturing

Electromagnetic stirring (EMS) continues to be a key component for raising efficiency and sustainability levels in aluminium manufacturing. ABB’s Frederik Esterhuizen reflects on how as the industry pursues decarbonization, proven technologies like EMS are delivering tangible, measurable results – now quantified through comprehensive lifecycle assessments.

Feature article

1970-01-01

This article was originally published in the November/December 2025 issue of Aluminium International Today magazine.

UNDERSTANDING THE ENVIRONMENTAL IMPACT

Aluminium production sits at the heart of industrial civilization and, simultaneously, at the center of the global carbon challenge. Despite its reputation as a ‘green metal,’ aluminium production remains energy intensive, responsible for roughly 2-3% of global CO₂ emissions. As governments and manufacturers worldwide set aggressive decarbonization targets, the aluminium industry faces the dual imperative of maintaining competitiveness while cutting emissions.

 

For the entire metals industry, what was once a traditional, conservative sector is now evolving rapidly. The drive for lower-carbon materials, transparency in supply chains and circular production models is reshaping expectations across the value chain. In this environment, ABB is taking a proactive role. Rather than waiting for regulation or customer demand to define new standards, ABB is advancing its own sustainability agenda, aligning with its Science Based Targets initiative (SBTi)-approved pathway and 2030 circularity goals to lead the metals industry toward verified, measurable metrics.

 

To meet these demands, progress increasingly depends on understanding a technology’s environmental impact across its entire existence, from manufacturing through decades of use and eventual recycling. ABB’s recent lifecycle assessment (LCA) for its electromagnetic stirrer for aluminum furnaces (AL-EMS) marks a major step in this direction. The initiative forms part of ABB’s broader effort to quantify and minimize the full environmental footprint of its products, using the LCA as a scientific measurement tool to understand its impact.

 

 

Following ISO 14040 and ISO 14044 methodology standards, this assessment provides a cradle-to-grave understanding of environmental impact, assessing three distinct lifecycle stages from raw material extraction through production, operational use and end-of-life treatment. The findings reaffirm a fundamental reality of industrial equipment: in long-lived technologies, the use phase dominates total environmental impact. The energy consumed over a 20-year operational life outweighs the embodied impacts of manufacturing or transport.

 

This insight strengthens the business case for technologies that improve process efficiency. Every percentage point of energy saved in aluminium production compounds over thousands of heats and melts, delivering environmental benefits that far exceed the footprint of producing the equipment itself.

 

Production at ABB’s Västerås facility in Sweden is powered entirely by renewable hydropower, while waste metals from manufacturing are recycled or responsibly disposed of. At end-of-life, the high steel and copper content in electromagnetic stirrers – 82% in the aluminium furnace stirrer – enables substantial material recovery.

 

Beyond demonstrating environmental performance, the LCA provides strategic direction for ongoing improvement. The lifecycle data clearly identifies where interventions deliver the greatest environmental benefit, guiding decisions on material selection, supplier engagement and product development priorities. This evidence-based approach ensures that development efforts target the stages of a product’s life where reductions in environmental impact will be most significant.

EMS THROUGH THE LIFECYCLE LENS

As the inventor of AL-EMS, ABB has pioneered its use in metallurgical operations since the 1960s, yet its potential impact on energy efficiency has only recently gained renewed focus. The technology uses magnetic fields to induce controlled motion within molten metal, creating a stirring force without physical contact. This homogenizes temperature and chemical composition, eliminating cold or stagnant zones that would otherwise cause inefficiencies.

 

In aluminium manufacturing it plays an important role in melting, holding and refining furnaces. These operational benefits directly support the environmental performance trends identified through the LCA process: efficiency in the use phase is where the greatest gains are achieved.

 

Aluminium of Greece, for instance, increased the proportion of solid material in its melts, effectively enabling a higher share of recycled scrap, while simultaneously boosting furnace productivity using AL-EMS. Nordural in Iceland adopted the same technology to improve temperature uniformity in its holding furnaces, allowing the use of harder, more cost-effective alloys and enhancing overall operational flexibility, resulting in a 17% improvement in productivity at the site.

 

The process benefits are tangible: reduced thermal differences, efficient homogenization of alloying elements and lower specific energy consumption. These gains translate directly into lower emissions because they enable operators to use a higher proportion of recycled, secondary aluminium, which itself requires only around five percent of the energy needed for primary production. By stabilizing the melt and ensuring uniform alloy composition, AL-EMS makes it possible to incorporate more scrap material without compromising product quality, helping to unlock the full carbon advantage of secondary metal.

 

 

Proven technology for a sustainable future

Lifecycle transparency is increasingly characterizing industrial sustainability. Market mechanisms such as carbon pricing, emissions trading and customer demand for verified low-carbon metals are turning environmental performance into a competitive differentiator. For metals producers, operational excellence now also includes sustainability excellence.

 

The aluminum industry’s decarbonization pathway combines multiple strategies – increasing the proportion of secondary metal, electrifying refining operations and improving operational efficiency. However, such transitions will take years to achieve at scale. Aluminium producers can make meaningful progress today using solutions that fit seamlessly into their current operations. AL-EMS is one such technology. It can be applied to both new and existing furnace installations, whether side- or bottom-mounted, liquid- or air-cooled, offering flexibility across a wide range of configurations. This adaptability means producers do not need to replace core furnace infrastructure to realize energy and emissions savings. With its proven performance, low implementation risk and measurable payback period, AL-EMS provides a practical, scalable route toward lower-impact aluminium production.

 

Looking ahead, continuing innovation in electromagnetic stirring, including improved coil designs, adaptive control algorithms and remote support capabilities, will further enhance process flexibility and decarbonization. In this sense, AL-EMS demonstrates that decarbonization need not rely solely on breakthrough innovations. Established technologies, when refined and applied intelligently, can yield immediate gains while enabling longer-term transformation – a pragmatic approach that resonates with metals producers pursuing realistic, proven pathways to emissions reduction.

LEARN MORE

Electromagnetic stirrers and brakes

Improving furnace efficiency and continuous casting quality

AL-EMS electromagnetic stirrer for aluminium furnace

Enhance furnace productivity while reducing dross and energy consumption

ABB in Metals

ABB is a trusted partner and leading supplier to the metals industry, delivering a broad portfolio of integrated electrification, automation, metallurgical and digital solutions.

ABB's 2030 sustainability strategy

With our leading technologies in electrification and automation, we are at the core of accelerating the energy transition. We help all industries run at high performance and become more productive, efficient and sustainable so they can outperform.