PMA PRODUCTS CONFORM TO WORLDWIDE STANDARDS AND REGULATIONS.
As a pioneer in the field of cable protection, PMA AG exercises a significant influence on the development of international standards. Standards committees with responsibility for cable systems regularly ask our company to provide advice or participate as an active member.
The Swiss Electrotechnical Association Electrosuisse is a testing centre for safety-related examinations with the accreditation to carry out examinations of all relevant EN and EC standards for low voltage-manufacture like components, appliances, installations for electro and communication economy and to prove the conformity of the products (accreditation number STS 001). As well as their own internal laboratory, the Electrosuisse is, as an internationally active company, an important partner for the PMA AG regarding products and material examinations.
A world-leading manufacturer of innovative transportation solutions, from regional aircraft and business jets to rail transportation equipment, Bombardier Inc. is a global corporation headquartered in Canada. PMA products are successfully used by Bombardier in many rail transportation applications. They comply with the demanding specification requirements by Bombardier.
The "Laboratoire National d'Essais" (LNE) is a testing centre with the accreditation to carry out tests and to prove the conformity of products according to many different standards and individual specifications. As well as their own internal laboratory, the LNE are an important partner for PMA AG regarding fire protection technical product examinations in accordance to international standards.
Lloyds Register (LR) is an independent classification and inspection authority for the shipping and machine construction industry. Type approval certificates regarding the LR requirements for the use in the shipbuilding and Off-Shore area are available for various products of the company PMA AG.
www.lr.org
CSA (Canadian Standard Association) is editor of different product standards. CSA tests the characteristics of products and systems in order to guarantee that these comply with the requirements of the Canadian market. The PMA product portfolio comprises a large choice of conduits and connectors which are tested and surveyed by CSA.
ALSTOM designs, builds and services technologically advanced products and systems for the world's energy and transport infrastructure. PMA products are the preferred System for rail transportation systems and marine branch applications due to Worldwide approvals and experiences with the products.
The Deutsche Bahn AG maintains among others also own fire technical testing laboratories. The flame properties of different PMA products are tested and classified according to current standards by the Deutsche Bahn.
L'Union Technique de l'Automobile du Motocycle et du Cycle" (UTAC) is an independent, technically specialized testing centre for the certification and admission of products in the automobile area.
A global player covering different business fields such as Automation and Control, Information and Communications, Medical, Power and Infrastructure, Rail Transportation and Services. Siemens Transportation groups' products and solutions are designed to provide mobility for a world on the go and to meet growing demands for environmental compatibility and improved performance. PMA is proud to be a first source supplier for the Siemens Rail Transportation Systems. Also other business fields count on beneficial characteristics of PMA products.
A world-leading manufacturer of innovative transportation solutions, from regional aircraft and business jets to rail transportation equipment, Bombardier Inc. is a global corporation headquartered in Canada. PMA products are successfully used by Bombardier in many rail transportation applications. They comply with the demanding specification requirements by Bombardier.
The "International Electrotechnical Commission" IEC is an international standards and conformity assessment body for all fields of electrotechnology.
UL (Underwriters Laboratories) is editor of different product standards. UL tests the characteristics of products and systems in order to guarantee that these comply with the requirements of the American market. The PMA product portfolio comprises a large choice of conduits and connectors which are tested and surveyed by UL. The symbol above indicates that products have been tested at UL according to the requirements of the Bi-National cable protection standard UL 1696 _CSA C22.2 No.227.3-05 and are approved for both USA and Canada.
Promoted by UNIFE and supported by operators, system integrators and equipment manufacturers, IRIS (International Railway Industry Standard) complements the internationally recognized ISO 9001 quality standard introducing rail specific requirements. IRIS is modelled on similar quality standards already in place in the aerospace, and automotive industries and it aims at the avoidance of multiple business management system auditing and therefore increased cost efficiency. Objectivity and transparency are guaranteed by only using approved and independent certification bodies, known and recognized in the industry.
The IRIS certificate will replace individual management system evaluations by at least the four founders of this initiative (Alstom Transport, AnsaldoBreda, Siemens Transportation Systems and Bombardier Transportation).
The French National Railway company S.N.C.F. is one of the leading authorities to develop and implement specification requirements for the European railway industry. PMA products have been approved by the French National Railway Company and is homologated for use on S.N.C.F train cars and Infrastructure.
UL (Underwriters Laboratories) is editor of different product standards. Furthermore, the UL tests and surveys the characteristics of products and systems in order to guarantee that these comply with the US American market. The PMA product portfolio comprises listed conduits and connectors which are tested and surveyed by UL.
The symbol above indicates that products have been tested at UL according to the requirements of the Bi-National cable protection standard UL 1660 - C22.2 No. 227.2.1-04 and are approved for both USA and Canada. "UL-Listed Products" are tested to a higher degree of safety than “recognized” products and can be sold for installation by untrained personnel in installations accessible to untrained personnel. A UL “Recognized” product is usually sufficient if the product is being installed into a fully enclosed system by a trained engineer.
During the last years the EC has issued for important product groups totally 20 guidelines according to the ”New Approach” which must be moved into national right by the member states of the European Union. The EC refers in these guidelines to the establishing of the basic technical requirements concerning security and health protection. To put the general legal requests into actual form, the EC engages the European Standardization Institutes (CEN, CENELEC, ETSI) with the creation of European Standards (EN). With the publication in the EC official gazette, these attain the status of harmonized standards. With the CE designation as well as the conformity explanation, PMA certifies the accordance of the relevant products with the requirements of the low voltage guideline (73/23/EEC).
London Underground Limited (LUL) is a subsidiary of London Transport. LUL is editor of a variety of product standards and specifications. Accredited testing centres according to the LUL specifications test the fire protection requirements for products and systems. Especially fire protected products from the PMA product range are used in LUL vehicles, tunnels or subway stations.
UK Conformity Assessed (UKCA) marking is a conformity mark that indicates conformity with the applicable requirements for products sold within Great Britain.
The UKCA marking became part of UK law at the end of the Brexit transition period, on 31 December 2020, with the coming into force of The Product Safety and Metrology etc. (Amendment etc.) (EU Exit) Regulations 2019. It has been mandatory since then, although, until 31 December 2024 (an extended deadline, which was previously 1 January 2022 then 31 December 2022), the CE mark is accepted as a valid alternative. The scope and procedures of the UKCA scheme will initially follow those for CE marking, but after 31 December 2020 the two schemes may diverge.
With the UKCA designation as well as the conformity explanation, PMA certifies the accordance of the relevant products with the requirements of the low voltage guideline.
Det Norske Veritas (DNV) is an independent classification and inspection authority for the shipping and machine construction industry. Type approval certificates regarding the DNV requirements for the use in the shipbuilding and Off-Shore area are available for various products from the company PMA AG.
CSA (Canadian Standard Association) is editor of different product standards. CSA tests the characteristics of products and systems in order to guarantee that these comply with the requirements of the Canadian market. The PMA product portfolio comprises a large choice of conduits and connectors which are tested and surveyed by CSA.
German industry norm / association of the electo-technology electronics information technology e.V.
ABS (American Bureau of Shipping) is an independent classification and inspection authority for the shipping industry. Type approval certificates regarding the ABS requirements for the use in the shipbuilding and Off-Shore area are available for various products from the company PMA AG.
Trenitalia is the operator of goods and passenger transport within Gruppo Ferrovie dello Stato (FS), the Italian railway company. Based on various standards like fire protection standards Trenitalia specifies and qualifies suitable materials for rail vehicle engineering.
Gost in the Cyrillic language means standard. In 1989 the Russian authorities introduced for the first time regulations related to quality control for products manufactured and sold within the country. The regulations were first implemented in the early 1990Ãs providing the legal and technical foundation for the national certification system. From 1992 the directives were put into practice.
Products manufactured within or imported into the Russian federation should be certified. The Gost-R certificates can be compared to the European CE declaration of conformity system, with the difference that the CE system is based upon self certification. It is the responsibility of the manufacturer to ensure that his product complies with all the relevant standards, whereas a Gost certificate may only be issued by a registered authority.
MORE ABOUT PMA SUSTAINABILITY ACTIONS
As a technology leader in electrification, ABB is at the core of accelerating the energy transition. Every day, we empower customers across the globe to optimize, electrify and decarbonize their operation. Learn more about PMA other sustainability actions.