ABB INFINITUS: DESIGNED TO POWER THE DIRECT CURRENT REVOLUTION

ABB Infinitus Direct Current portfolio complements traditional AC systems, enabling greater power density, efficiency, reliability, and scalability for AI-era data centers.

ABB INFINITUS: THE INDUSTRY’S FIRST SOURCE-TO-RACK DIRECT CURRENT PORTFOLIO FOR AI DATA CENTERS

The Infinitus portfolio provides the building blocks for DC-native and hybrid AC/DC data center architectures, helping data center operators improve energy efficiency, reduce power infrastructure footprint, and support greater computing capacity.

 

At the heart of the portfolio is the ABB Infinitus solid-state transformer (SST), designed to convert medium-voltage AC power to 800 VDC with fewer conversion stages. 

 

Infinitus brings together power conversion, power quality, distribution, protection and cooling optimization in a coordinated architecture designed for efficient, reliable, and scalable AI infrastructure.

ABB's DC leadership, backed by scale

Decades of direct current expertise, backed by continued investment in direct current technology, testing, manufacturing capacity, R&D and industry collaboration.

700+

DC Patents

25 Years

DC Leadership

40%

of electrification R&D dedicated to next-gen technologies and DC innovation

FIVE KEY BUILDING BLOCKS

Engineered for efficient, reliable AI infrastructure at scale.

AN INTEGRATED PORTFOLIO SUPPORTING FLEXIBLE 800 VDC ARCHITECTURES

MV Powertrains

Grid Support solutions

Help data centers manage voltage stability, frequency response and rapidly changing AI loads. Synchronous condensers, battery energy storage systems and services, and advanced controls support power quality, grid compliance, and resilient operation.

MV Switchgear

Provides primary distribution (UniGear and ZX portfolio) and secondary distribution (UniSec and SafeRing/SafePlus offering) grid-facing protection, switching, monitoring and control. Gas insulated compact and air insulated modular solutions, coming with arc-resistant designs supporting enhanced operator safety.

HiPerGuard MV UPS

The industry’s first static medium-voltage UPS designed for hyperscale data centers. Direct 34.5 kV grid connection reduces conversion losses and infrastructure complexity.

Delivers stable, resilient power from the grid or on-site generation, with technologies that support power quality, protect critical infrastructure, and help manage rapidly changing AI loads. 

Converts AC power to 800 VDC outside the white space, reducing conversion stages while supporting efficient power delivery and power quality for high-density AI infrastructure in a smaller footprint.

Delivers power safely and reliably, enabling higher power density in less space. Receives and distributes high volumes of 800 VDC to meet the power demands of AI compute rows.

Provides protection for operators, AI servers and hardware from DC fault currents overcurrents. Instant selective interruption safeguards assets while keeping the system online.  

Reduces the energy consumed by the full cooling chain across grey and white space, supporting efficient and reliable operation of high-density AI infrastructure.

3D illustration of a data center building with server racks, cooling units, and glowing electrical connections visualizing power distribution and data flow across the facility.

Ready to lead your industry into the Direct Current era?

Experience the Infinitus DC portfolio, and discover resources for next-generation data center infrastructure.

Access the immersive ABB Infinitus Experience Close-up of a large digital monitoring dashboard displaying interconnected data flows, charts, and system metrics on a screen in a modern control room.

ABB Data Center Solutions

Explore how ABB technologies and people make data centers more efficient, reliable, and scalable.

The Strategic case for Hybrid AC/DC Power

Explore the ABB and BCG report on the growing role of direct current in future power systems 

"ABB has pioneered DC technology for more than 25 years across several segments. The Infinitus DC portfolio is expected to drive similar benefits across other energy-intensive industries including manufacturing, renewables, and marine operations."

Giampiero Frisio, President, ABB Electrification

HIGHLIGHTS

ABB’s new DC portfolio aims to rewire AI data center energy infrastructure

ABB joins forces with Ferrari Hypersail to take Direct Current to new horizons

ABB/BCG report highlights growing role of DC technologies in future power systems

ABB launches the industry's first source-to-rack direct current portfolio

ABB to develop next-generation AI data centers with NVIDIA

ABB to acquire Advantics, expanding Direct Current portfolio

Redefining power infrastructure for AI: the role of 800 VDC in data centers

How direct current technology will power the energy transition

FREQUENTLY ASKED QUESTIONS

The Infinitus DC portfolio is an integrated source-to-rack direct current power portfolio for AI data centers. It brings together the building blocks needed for DC-native and hybrid AC/DC architectures, including medium-voltage powertrain solutions, 800 VDC power conversion, power quality, distribution and protection solutions, and cooling optimization technologies. 

The Infinitus DC can deliver efficiency gains of more than 5%, helping reduce end-to-end energy and heat losses, conductor and copper requirements, and power infrastructure footprint. This enables reliable, high-density power delivery while making more power and space available for computing. 

The Infinitus DC portfolio is the industry's first integrated source-to-rack DC portfolio. At its core is ABB’s breakthrough Infinitus solid-state transformer (SST) technology, enabling sites to operate with a smaller footprint and greater energy efficiency. As the only major electrification supplier with both the world's first fully IEC-certified solid-state circuit breaker and an industry-first static medium-voltage UPS in production, ABB delivers a breadth of technology unmatched in the market. 

800 VDC enables higher power transfer at lower current, helping to reduce conductor requirements, distribution losses and infrastructure footprint. NVIDIA introduced the architecture for future megawatt-class AI systems. In October 2025, ABB announced a collaboration with NVIDIA to support the development of 800 VDC power architectures for next-generation AI data centers. The wider industry is increasingly aligning around 800 VDC through initiatives such as the Open Compute Project (OCP). While higher voltage levels may emerge as power requirements evolve, 800 VDC provides a practical common foundation for the next generation of AI data centers.  

The Infinitus solid-state transformer (SST) converts medium-voltage AC power directly to 800 VDC using high-frequency solid-state power conversion, helping reduce conversion stages, energy losses, and infrastructure footprint. 

As AI data centers become more compute-intensive, efficient cooling is essential to performance and uptime. ABB's high-efficiency motors and drives optimize pumps and cooling equipment, helping improve energy productivity while maintaining optimal thermal conditions. ABB's drive technology is also ready for emerging DC architectures, helping operators maximize the computing capacity they can deliver from every megawatt of available power.  

ABB provides electrification and automation solutions to help customers design, build and operate data centers that are more reliable, efficient and scalable. ABB has been a trusted partner in global electrification for over 140 years. Around the world, one in four data centers run on ABB technology. ABB brings over 25 years of applied DC technology deployment and over 700 DC patents. ABB works with hyperscalers and chipmakers, including NVIDIA, and collaborates with industry bodies, including the Open Compute Project (OCP), Open Data Center Alliance and Current/OS to shape standards.  

ABB co-leads the Open Compute Project’s (OCP) Data Center Facility Power Distribution subproject and leads its Protection and Safety workstream. ABB also participates in the Open Data Center Alliance and Current/OS, contributing to the specifications, safety requirements and interoperability needed for wider DC adoption. 

ABB is helping advance a future in which AC and DC architectures work together, with DC increasingly supporting high-density AI infrastructure where it creates the greatest value. Through Infinitus DC and industry collaboration, ABB is developing the technologies and standards needed for this transition.  

ABB expects that DC will play a growing role in energy-intensive applications where it offers clear technical and economic advantages. While data centers present the most immediate need, other energy-intensive industries, including manufacturing, renewable energy, marine operations, EV charging, and energy storage, could benefit from more efficient power conversion and distribution.