PMA® FLEXIBLE PROTECTION SYSTEM ECOGUARD
Our commitment to sustainable solutions for the industry.
PMA ECOGUARD™ SUSTAINABILITY IN CABLE PROTECTION
Enabling a more sustainable and resource-efficient future. Made from 50% recycled raw material, PMA EcoGuard™ is our commitment to sustainable solutions for the industry. PMA EcoGuard™ products are employed for maximum protection of the installation’s cable connections under rigorous conditions.
KEY FEATURES AND BENEFITS
<p>ABB's PMA EcoGuard system delivers high-performance cable protection crafted from ecycled polyamide, manufactured at ABB's facility in Uster, Switzerland, where sustainable design and rigorous performance testing go hand in hand.</p>
Environmentally responsible
<p>Made from 50% recycle-based polyamide sourced primarily from recovered fishing nets, reducing 30% of upstream Scope 3 CO2 emissions and 50% of net freshwater use compared to conventional alternatives.</p>Flexible
<p>RPPA conduit delivers very good flexibility and a temperature range of -40°C to +95°C continuous, making it well suited for machine building and renewable energy applications where space is limited or routing paths are complex.</p>Durable
<p>Very high impact resistance across RPPA conduit and BFH-RP one-piece system support ensures long-term mechanical performance in demanding industrial environments.</p>Easy installation
<p>BRND fittings feature a push-in installation design and BFHRP system support mounts with a single hole fixing, enabling fast setup without additional tools.</p>UV-resistant
<p>Good UV resistance and weathering characteristics support reliable performance in outdoor applications including wind parks and solar installations.</p>Chemical-resistant
<p>Very good chemical properties across conduit and fittings support use in industrial environments with exposure to oils, greases and other agents.</p>Compliant
<p>Certifications include ABB EcoSolutions, RoHS, REACH, UL2809 ECVP Ocean-Bound Plastic, CE and ISO 14044 third-party verified Lifecycle Assessment (LCA Type III)</p>
INDUSTRIES WE SUPPORT
From residential construction to commercial and industrial projects, our products support professionals across diverse industries.
Machine Building, Energy, Rail industry
CHALLENGES WE SOLVE
Our products are designed to help professionals solve installation, safety and performance challenges in demanding applications.
Sustainability, Liquid and dust exposure, Harsh environments
OUR STORIES: INDUSTRY NEWS AND INSIGHTS - OPTION 1
ABB AND LYONDELLBASELL
- ABB AND LYONDELLBASELL
- ABB AND ENVALIOR
FROM INDUSTRIAL PRODUCTION WASTE TO RAILWAY CABLE PROTECTION
LyondellBasell (LYB), one of the world's leading polymer manufacturers, is ABB's strategic partner for the recycled engineering material used in PMA EcoGuard™ VAML/RP conduit. Through its CirculenRecover™ portfolio, LYB helps transform industrial production waste into high-performance materials that support a more circular economy without compromising quality or performance.
For PMA EcoGuard™ VAML/RP conduit, LYB developed a dedicated engineering material grade using post-industrial recycled polyamide. Instead of relying solely on virgin fossil-based feedstocks, valuable production scrap and off-cuts are mechanically recycled and transformed into a high-performance material suitable for demanding railway applications. This approach keeps engineering materials in use for longer, increases the use of recycled content and contributes to reducing the environmental impact of the final product.
The CirculenRecover™ material provides long-term heat resistance, excellent flexibility, reliable processing and mechanical durability while complying with stringent EN 45545-2 HL3 railway fire safety requirements. Together with LYB, ABB is helping make railway cable protection more circular while maintaining the safety, quality and reliability expected by the rail industry.
FROM ABANDONED FISHING NETS TO ADVANCED CABLE PROTECTION
Envalior is ABB's strategic partner for the recycled engineering material used in PMA EcoGuard™ RPPA conduit. A leading global engineering materials solution provider, Envalior has a combined 100-year track record of customer-centered innovation, focusing its deep material and application expertise on sustainable high-performance products.
PMA EcoGuard™ PA6 cable protection boasts a remarkable feature — it is crafted from 50% recycle-based polyamide sourced primarily from abandoned nylon fishing nets. Instead of relying solely on virgin fossil-based feedstocks, recovered nets are sorted, cleaned, extruded and quality-inspected before being transformed into a high-performance engineering material. This approach keeps valuable materials in use for longer, increases recycled content and contributes to reducing the environmental impact of the final product.
The new PMA EcoGuard™ contributes to a substantial reduction in upstream Scope 3 greenhouse gas emissions by 30% and a 50% decrease in water consumption compared to conventional fossil feedstock-based alternatives. Together with Envalior, ABB is helping make cable protection more circular while maintaining the safety, quality and reliability expected across industrial environments.
OUR STORIES: INDUSTRY NEWS AND INSIGHTS - OPTION 2
LyondellBasell (LYB), one of the world's leading polymer manufacturers, is ABB's strategic partner for the recycled engineering material used in PMA EcoGuard™ VAML/RP conduit. Through its CirculenRecover™ portfolio, LYB helps transform industrial production waste into high-performance materials that support a more circular economy without compromising quality or performance.
For PMA EcoGuard™ VAML/RP conduit, LYB developed a dedicated engineering material grade using post-industrial recycled polyamide. Instead of relying solely on virgin fossil-based feedstocks, valuable production scrap and off-cuts are mechanically recycled and transformed into a high-performance material suitable for demanding railway applications. This approach keeps engineering materials in use for longer, increases the use of recycled content and contributes to reducing the environmental impact of the final product.
The CirculenRecover™ material provides long-term heat resistance, excellent flexibility, reliable processing and mechanical durability while complying with stringent EN 45545-2 HL3 railway fire safety requirements. Together with LYB, ABB is helping make railway cable protection more circular while maintaining the safety, quality and reliability expected by the rail industry.
Envalior is ABB's strategic partner for the recycled engineering material used in PMA EcoGuard™ RPPA conduit. A leading global engineering materials solution provider, Envalior has a combined 100-year track record of customer-centered innovation, focusing its deep material and application expertise on sustainable high-performance products.
PMA EcoGuard™ PA6 cable protection boasts a remarkable feature — it is crafted from 50% recycle-based polyamide sourced primarily from abandoned nylon fishing nets. Instead of relying solely on virgin fossil-based feedstocks, recovered nets are sorted, cleaned, extruded and quality-inspected before being transformed into a high-performance engineering material. This approach keeps valuable materials in use for longer, increases recycled content and contributes to reducing the environmental impact of the final product.
The new PMA EcoGuard™ contributes to a substantial reduction in upstream Scope 3 greenhouse gas emissions by 30% and a 50% decrease in water consumption compared to conventional fossil feedstock-based alternatives. Together with Envalior, ABB is helping make cable protection more circular while maintaining the safety, quality and reliability expected across industrial environments.