ARE RENEWABLES MAKING OUR GRIDS LESS RELIABLE?
A conversation with Adrian Guggisberg, Division President, Electrical Distribution Solutions, ABB
Hosted by Pamela Largue • In partnership with ABB
PAMELA 0:13
As more variable renewable energy is integrated into our transforming power system, one question continues to spark debate: Are renewables making our grids less reliable? To answer this question, I speak to Adrian Guggisberg, Division President, Electrical Distribution Solutions at ABB.
He references the Iberian blackout, highlighting key lessons about maximizing grid resilience, and emphasizes the consequences of increasingly complex power systems operating on infrastructure designed for a different era. From artificial intelligence to smarter distribution networks, Adrian explains why the energy transition demands a rethink of how grids are designed, monitored, and controlled. This episode is brought to you in partnership with electrification and automation specialists ABB. I am Pamela Largue, and this is the Energy Transitions Podcast.
Adrian, thank you so much for joining me today. We're talking about such an important topic: increasing renewable energy and the impact that is having on the grid. So, let's dive in.
Is the increased share of renewable energies causing grid issues? Are we seeing that renewables are actually responsible for blackouts?
ADRIAN 1:35
Hey, Pam. Thanks a lot for having me, first of all. It's a super valid question, and I think that people are getting maybe, in some places of the world, a bit worried about what it means to add so much renewable power into the power grid. Look, either way would probably be the wrong answer—to say “no,” and it would also be the wrong answer to say “yes, it is causing blackouts.”
What is a fact? Maybe to make a bit of an analogy: It's like, you know, if you had a car from the 1970s and you said, “Okay, let me now put the latest motor which I can find on the market into that same car, and let me drive as fast as I can.” I think that would not work well. Now, is the motor to blame because the car does not have good performance? Probably not. I think that the car as a design needs to fit together with the motor. So, a somewhat similar thing is happening: Our grids were built years ago, designed around having large, centralized, well-controlled power generation. Now, suddenly, we have a completely different scheme, and there is a lot of renewable power. It's very distributed. It behaves differently than the power generation for which the grid was originally designed would have behaved, and the combination can now cause new challenges.
PAMELA 2:40
New challenges, indeed! But what a great analogy. Just for breaking that down for us, Adrian, I'd like to hone in specifically on the Iberian blackout, which surprised many because it wasn't actually caused by an equipment failure. So, what was the role, then, of renewable energy in this? What else actually caused the blackout if it wasn't renewables?
ADRIAN 2:58
Yeah, I think probably many people have watched the analysis of what happened there very carefully, and I think there was a report published a few weeks ago on the detailed analysis. Obviously, there's kind of a very complex scheme, it's not super simple, and there are many elements. But let me try to summarize a bit of the main learnings, at least the way I would look at this.
What we saw from the report and from those learnings: The first point was actually that there was really a lot of renewable power in the grid, which kind of supplied energy into the grid. That was one element. The other element was that the renewable power, where it was generated, was not necessarily where the power was consumed. So, it was transferred over quite some distances within the Iberian Peninsula, and that kind of was, let me say, the starting point.
Now, what happened is, at one operating point, the grid started to oscillate. Oscillations—you all understand from music when there is a sound where a tone goes up and down and so on. So, the energy started to oscillate. Now, that's a very dangerous situation for a grid. In that respect, it's not something which people would be overly concerned about, but one needs to act, and the grid operator acted. They reconfigured the grid. By reconfiguring the grid, you're changing the behavior of the grid. That oscillation went away, but by this reconfiguration of the grid, actually, something else was caused, and there was another oscillation. Actually, a known oscillation was triggered, which they say is actually in between the continents—it's called a west-east oscillation or mode. For that, there are kind of predefined procedures on how to act when this happens. And then, the procedure was again to do some reconfiguration of the grid, now to deal specifically with that problem.
That's kind of the starting point of everything. Now, with that reconfiguration, what happened is actually, on the Iberian Peninsula, the voltage control got out of balance. Voltage control—and now I'll make a little bit of an excursion—is what you do on the grid when you control two things: You control the power, and you control the voltage. The voltage control went out of balance. The voltage started to increase in the grid, especially in some of the nodes. And at one point, now the third thing started to happen. Actually, some of these nodes started to be disconnected because they said, “I need to protect myself; the voltage gets too high.” And now they disconnected. By disconnecting some of the nodes, actually, the situation got worse, and the voltage got even higher in other places. And now we had an avalanche. The avalanche is just: More nodes get disconnected, higher and faster the voltage goes up, and more gets disconnected until everything shuts down.
Again, kind of the first thing: We had a situation with a grid connection which was not the way the grids were designed many years ago—a lot of renewable power generation, distributed power, and the power demand was in different places. Second thing: We got some oscillations on the systems. Then procedures were applied which were designed to deal with this specific problem. But with that problem, we introduced a new problem, and that new problem created an avalanche through the decentralized protection because it got completely out of balance.
These were kind of the three major steps which happened in the grid.
PAMELA 6:46
So it really was a perfect storm, like you say—an avalanche. But it seemed to be a series of correct actions rather than mistakes that caused such a failure.
Did the protection and control schemes all work correctly as intended?
ADRIAN 7:05
Partly yes, and partly no. I would say probably we can distinguish three things.
There was one thing—the first thing: There were procedures applied on how to reconfigure the grid, and those procedures were applied the right way in terms of how they were designed, but they were not necessarily designed for the grid of today. They were very much designed for the grid of the past. So, that's the first thing.
The second thing would also be what I mentioned before: Some of the nodes were turned off because of overvoltage, but the analysis found out that, actually, some of the settings out there in the grid are not according to the definition of the settings. So, some settings were too low, which caused some of the nodes, actually, to switch off too early, which didn't give the time to react in a different way. That was a little bit of the second thing, where I would say it was not quite as it should be.
And then the third thing is more of a missed opportunity, and the missed opportunity is basically that the renewable power sources could be used to control the voltage. They are not. They are just operated in a fixed scheme. So, the voltage control was relied on at a few points in the grid instead of really using all the capabilities that are there.
So, that's kind of three things: One a missed opportunity, one probably something which is not up to speed, and one was not exactly as it was designed. So, kind of three factors here.
PAMELA 8:38
My next question, then, is: Okay, what do we do about this? How do we address these three points that you've identified?
ADRIAN 8:46
Yeah, I think for me, the big conclusion out of that event is that we need to rethink grid resilience. I would say, for many years, we have defined grid resilience by the quality of equipment; we have looked into the structures of the network, but I think that's not enough anymore today.
PAMELA 9:02
Would you say, Adrian, that digitalization is actually no longer an option, but it's actually essential to ensure real-time grid intelligence? And do you think something like this could have actually impacted the outcome of the Iberian blackout?
ADRIAN 9:18
Absolutely. Yes, I think this is really the part which is probably the biggest step we need to take when we rethink the electrical grid: I think it needs to be digitalized.
Now, I would say, you know, if you go into the high-voltage level where you see these transmission lines, that level, I think, is quite well digitalized and is also controlled. That's the way the whole grid was controlled in the past. But now, as we have way more decentralized power sources with more renewables, with energy storage systems, and also with dynamic loads, a distribution network—which is one layer below the high-voltage network—needs to also become more intelligent and needs to be controlled in a different manner. So, digitalization absolutely is a must. Without that, I think we will not be able to get the resilience we are looking for.
PAMELA 10:13
A good segue into my next question, because with digitalization, we have to talk about artificial intelligence, which seems to really be upping the game in terms of grid intelligence. My question is: Where do you see the biggest opportunities for AI, but also advanced analytics and autonomous grid control, in terms of improving resilience over the next decade?
ADRIAN 10:26
I think here, probably the obvious part is, you know, as we have a much higher complexity in this network—and you can imagine, you know, on the high-voltage lines, there are a few, but if you go down in the voltage levels closer to the consumers, there are millions of kilometers of lines and thousands of connection points—now, this complexity is way too high for humans to look at data and then make good decisions. And here, it's a must, I believe, that we're going to use artificial intelligence in order to help us look into scenarios, saying: “If we do the following action, what will be the implications of these actions in order to get the best outcome?” And I think, here, technologies like artificial intelligence are super key in order to make this happen and to make this happen really in a good way.
PAMELA 11:21
Adrian, in your opinion, what are the biggest challenges to deploying this kind of intelligence? Because, obviously, we have the equipment and the technology—it already exists. So, where are we experiencing the bottlenecks in terms of deployment?
ADRIAN 11:33
Yeah, I think it's probably more the complexity of the entire ecosystem that we have today. So, you know, in Europe, you have literally hundreds of grid operators on the distribution grid. If you go to the transmission grid, there are a few.
So, the coordination among them—and the coordination among them with the policymakers—was quite easy compared to the problem we are facing now. Now we have hundreds of stakeholders, and the whole thing will only work if we can agree on certain standards and agree on certain procedures for how we do that. Otherwise, it's super hard to deploy any solution. So, as you can imagine, a little bit like... you know, if somebody in Belgium would decide, “Okay, we control it like this,” and then it looks and works like that, and then in Germany, again, three different methodologies, but everything is connected with each other—there, I think we need to agree on certain standardizations and certain approaches so that people can deploy the solutions in an effective way. Otherwise, it's going to be super slow and remain on a proof-of-concept level.
PAMELA 12:44
Obviously, standardization is critical, but also, potentially, sort of market and regulatory mechanisms as well. So, as distributed energy sources, EVs, and large data centers become active participants in the grid, how should grid codes and market regulations evolve to unlock their potential and actually support system stability?
ADRIAN 13:11
Yeah, probably it all starts with recognizing the challenge, and recognizing the challenge is always the first step in order to find solutions. And then, the other part is probably to rethink, again, a little bit about how policies and standards need to go.
If we stay on a super high level, we will obviously not be able to achieve a very good result. If we go too deeply prescriptive, everybody is worried about kind of taking the market or the market dynamics out of the equation and having it all regulated. To find this balance, I think that's going to be the big challenge. So, on one hand, we cannot stay on a super high level; otherwise, we are not creating a platform where things can be effectively deployed. On the other hand, if we go too granular, then I think we are just destroying the market dynamics.
PAMELA 14:04
Wise words indeed, Adrian. If we look beyond the Iberian blackout, what do you believe is the single biggest lesson utilities around the world should take away from this event, and what actions should they prioritize over the next five years to avoid a similar scenario?
ADRIAN 14:19
I think everybody needs to recognize that the distribution grid needs to change. So, the distribution grid cannot be built the way we have built it in the past. To make it more intelligent is, I think, number one. And then the second thing is really to also rethink whole resilience and what that means. So, I would say that's something I think people should take from this blackout, and also really to go deeper, I think, and really understand these dynamics which we also talked a little bit about, in order to deploy solutions which mitigate that for the future and also help us to build a way more resilient grid.
PAMELA 15:06
Adrian, my final question to you is: I'd like to find out what it is about working in this space that really keeps you motivated and involved, and would you say that you're feeling positive and encouraged about the work that's being done towards achieving greater grid resilience?
ADRIAN 15:22
I mean, it's a super cool field. I can only say that electrifying the world is probably one of the most important things we are doing. It's the tool to decarbonize the world, and if there is one challenge across the globe which unites us, I think we need to decarbonize this world. If we don't do that, there is no future for some of the generations to come. So, I think it is probably the number one topic. You know, we can talk about wars, we can talk about things which are bad in this world—I don't think humanity as such will suffer across the globe the same way. But with this one, we are all in the same boat. So, this is super cool.
The part which I think is something that at times makes you feel a little bit kind of tense: It would be nicer to go at a higher speed to deploy new ways of doing things, and also, probably, find ways in order to make this actually happen even faster than what we see today.
You can look at some of the reports, like from the International Energy Agency, which would also show that in some parts of the world, actually, you know, we have created enough renewable power, but we are not able to connect it to the loads, and we are not able to use it because the grid is transforming too slowly. So, these are the things which I would say, on one hand, are super cool. On the other hand, when you see it, you think like, “Oh, why can we not do that faster?”
PAMELA 16:47
Oh, I think you speak on behalf of so many people, Adrian, who absolutely agree with you on the need for speed. But for now, I really appreciate the fact that you took your time to share your insights with us. It has been such a pleasure. Thank you for joining us.
ADRIAN 17:00
Thanks, Pamela. Thanks a lot.
PAMELA 17:02
And thank you, and thank you to our listeners. Until next time, goodbye.