The energy trilemma in practice: how to manage the pressure affecting key global sectors
The energy transition, digitalization and geopolitical uncertainty are no longer parallel trends. They are converging, and the pressure is showing up in the same place across every sector: electrical infrastructure.
Webpage
1970-01-01
THE ENERGY TRILEMMA IN PRACTICE
- Pressure on industry and infrastructure: The energy transition, digitalization, and geopolitical uncertainty are placing unprecedented pressure on legacy electrical infrastructure across all sectors.
- The trilemma reality: Businesses are facing the immediate, daily operational challenge of balancing energy reliability, affordability, and sustainability simultaneously.
- Outdated maintenance: Aging assets and rising power demands are converging much faster than traditional "run-to-failure" maintenance strategies can handle.
- A new asset strategy: Achieving operational certainty requires a fundamental shift: treating electrical infrastructure as a flexible, strategic asset rather than a sunk cost.
- Proactive stewardship: Transitioning to proactive asset stewardship and targeted internal upgrades can slash unplanned downtime by up to 90% and allow operators to retain over half of their existing equipment indefinitely.
WHY ELECTRICAL INFRASTRUCURE RESILIENCE MATTERS
The energy transition, digitalization and geopolitical uncertainty are no longer parallel trends. They are converging, and the pressure is showing up in the same place across every sector: electrical infrastructure.
What once sat in the background as a stable, predictable backbone is now under strain. Demand is rising faster than capacity; regulatory requirements are tightening; assets are ageing. And the expectation of uninterrupted uptime has never been higher.
This is the energy trilemma in practice. Businesses are being asked to balance reliability, affordability and sustainability at a pace and scale that traditional maintenance models and investment cycles were never designed to handle.
Across utilities, manufacturing, oil and gas, buildings and data centres, the question is shifting from long-term strategy to immediate operational reality. How do you keep critical systems running while upgrading them, decarbonizing them and extracting more value from them at the same time?
SECTOR: UTILITIES
<p><b>The challenge for maintaining grid reliability while integrating renewables</b></p> <p>How do utilities maintain the infrastructure on which every other sector depends? And how do they manage the simultaneous pressure of integrating intermittent renewables, replacing aging distribution assets, and meeting near-perfect uptime obligations for industrial and domestic customers? The issue for utilities is that the infrastructure deficit sits squarely on their balance sheet.</p> <p><b>What ABB sees</b></p> <p>More than half of electrical equipment – metal cabinets, steel plates, busbars – can be retained indefinitely if the active internal components are regularly upgraded. Replacing outdated switchgear and circuit breakers with intelligent, monitored alternatives has delivered energy capacity improvements of up to 20 percent and operational cost reductions of up to 30 percent in real-world utility operations. Electric grids can also become more robust and capable of faster responses to outages through better use of fault detection, isolation, and restoration technologies.</p> <p><b>In practice: delivering capacity and cost improvements</b></p> <p>Finland’s <a rtestyle="text" class="cmp-richtexteditor__textlink" href="https://new.abb.com/news/detail/102904/european-hydropower-leader-on-top-of-the-world-with-leaner-sf6-free-retrofit-solution" target="_blank">Kemijoki hydropower company</a> retrofitted SF6 switchgear dating from 1995 and 2001 with vacuum circuit breakers. Downtime was measured in hours rather than weeks. The outcome addressed operational reliability, regulatory compliance (SF6 phase-out obligations under EU F-Gas regulations), and carbon footprint simultaneously.</p>
SECTOR: MANUFACTURING – CHEMICALS, STEEL, CEMENT
<p><b>The challenge: reducing energy cost and unplanned downtime</b></p> <p>How do ‘hard-to-abate’ manufacturing sectors deal with the energy trilemma given their energy intensive operations? </p> <p>These are typically 24/7 operations where energy represents 30–50 percent of total production cost, production stoppages trigger complex restart sequences, while decarbonization obligations under the EU Emissions Trading System, the Industrial Emissions Directive, and CSRD reporting are tightening steadily.</p> <p><b>What ABB sees</b></p> <p>A cultural barrier cuts across every hard-to-abate sector: KPI-driven short-termism. The plant manager’s success metric is units off the production line. Everything else – energy cost, maintenance cycles, asset health – is secondary until failure occurs. The result is a “run to failure” culture. On ABB’s own research data, that culture costs up to ten times more than a proactive maintenance strategy. The alternative – a shift from capital replacement to asset stewardship – delivers operating cost reductions of up to 33 percent, maintenance cost reductions of up to 85 percent, and reduces downtime by up to 90 percent.</p> <p><b>In practice: shifting from reactive to predictive maintenance</b></p> <p>At North American steel producer <a href="https://new.abb.com/news/detail/107690/arc-furnace-breaker-upgrade-forging-stronger-production-future-for-north-american-steel-giant">Finkl Steel,</a> a targeted switchgear upgrade halved the number of circuit breakers required, reduced maintenance costs significantly, and introduced 24/7 predictive health monitoring with accurate network synchronization. </p>
THE FUTURE OF ELECTRIFICATION SERVICE: 2026–2035+
<p>A roadmap for achieving operational certainty, energy resilience and business continuity in an increasingly complex energy landscape.</p> <p> </p>
SECTOR: OIL, GAS AND MINING
<p><b>The challenge: reducing carbon intensity while maintaining uptime in complex operations</b></p> <p>How are oil, gas and mining operators reducing carbon intensity of production, while maintaining uptime and resilience? </p> <p>Oil and gas operators are simultaneously managing the consequences of elevated commodity prices, the drive to electrify their own operations, and the need to reduce the carbon intensity of production. For mining, the additional challenge is reliability in remote, often single-feed operations where a production stoppage can have global supply chain consequences.</p> <p><b>What ABB sees</b></p> <p>Offshore platforms in Norway are increasingly powered by subsea cables from shore rather than onboard diesel generators – reducing both emissions and fuel logistics. A refinery now captures methane that would previously have been flared, uses it to generate electricity, and stores the output in battery systems that trade into peak energy markets – turning a waste stream and potent carbon emission into a revenue source. </p> <p>For mining, energy storage advisory work supports the development of microgrid solutions combining on-site renewables with battery storage, thus reducing diesel dependency and supply chain exposure in remote operations. The need for reliability is acute: a mine with a single power feed has no redundancy, and the shift from reactive to predictive asset health monitoring is a resilience requirement, not merely an efficiency gain.</p>
SECTOR: CRITICAL BUILDING INFRASTRUCTURE
<p><b>The challenge: managing rising energy demand, ageing assets and reliability expectations</b></p> <p>Is battery energy storage the silver bullet for reliable and resilient electrical power in buildings?</p> <p>Hospitals, airports, commercial buildings and large industrial facilities share a common set of pressures: aging electrical infrastructure, rising energy costs, growing EV charging loads, increasingly demanding HVAC requirements, and new embedded generation assets that were not part of the original design brief. For many of these facilities, battery energy storage is becoming the practical solution that ties these pressures together – smoothing grid volatility, supporting EV charging infrastructure, and enabling on-site renewable generation to be stored and deployed when it is needed most rather than fed back to the grid at negligible rates. Yet the sector receives far less attention than utilities or heavy industry when it comes to innovative energy solutions – despite facing the energy trilemma with equal intensity. </p> <p><b>What ABB sees</b></p> <p>A large facility – an international airport, a hospital campus, a major logistics warehouse hub – may contain tens of thousands of motors driving conveyors, HVAC, and cooling systems. Each is a potential failure point. But each, if monitored intelligently, is also an opportunity for proactive intervention that prevents the failure from happening. This has played out recently with an international airport that began with an exploratory discussion with a C-suite executive and concluded with a substantial project covering energy storage, microgrid design, and solar integration to boost the facility’s energy resilience.</p> <p><b>In practice: digital asset monitoring and smarter infrastructure</b></p> <p>Hospitals represent a particularly high-stakes environment. <a href="https://new.abb.com/news/detail/109137/largest-hospital-area-in-finland-modernizes-its-power-systems-to-ensure-mission-critical-uptime">Meilahti Hospital</a> in Helsinki used ABB’s digital monitoring and asset management solutions to future-proof its power supply, eliminate SF6 gas from its switchgear, and extend the useful life of its electrical infrastructure. This project is also delivering improved resilience and reduced environmental footprint without disrupting clinical operations.</p>
SECTOR: DATA CENTERS
<p><b>The challenge: ensuring uptime in AI-driven, high-density environments</b></p> <p>Have data centers become essential elements of critical national infrastructure? </p> <p>AI development, cloud computing, and the digitalization of public and private sector operations – including the military – depend on continuous, reliable operation of data centers. Power density is increasing with every new GPU generation. Hyperscalers routinely build facilities requiring over 100 MW of power. Uptime requirements for AI inference workloads can be measured in seconds – and in environments where a single outage affects millions of simultaneous users, financial, reputational, and contractual consequences compound rapidly.</p> <p>This is why modernizing electrical infrastructure is no longer optional. For data center operators, the question is not if they can afford to invest in electrical modernization – but whether they can afford not to.</p> <p><b>What ABB sees</b></p> <p>ABB’s research shows unplanned outages can cost around $125,000 per hour, and for data centers, even minutes of downtime can mean millions in losses. The impulsive load behavior of AI workloads – cycling from near-zero to full draw in milliseconds – creates power quality challenges that conventional switchgear, uninterruptible power supplies (UPS), and cooling systems were not specified to handle. Many existing facilities continue to operate with electrical infrastructure installed decades ago, in a different computing era.</p> <p>It is not surprising, therefore, that <a href="https://datacenter.uptimeinstitute.com/rs/711-RIA145/images/2024.Resiliency.Survey.ExecSum.pdf">according to Uptime Intelligence</a>, failures in on-site power distribution equipment are the most common cause of severe outages and the industry and regulators are concerned about the effects of these incidents. Other causes – failures in cooling systems – can be ridden through for a period while workarounds are found, while IT outages are often isolated, rather than system-wide.</p> <p>The challenge is not only capacity. It is resilience, efficiency and the ability to integrate renewable energy at scale. Keeping existing data centers up and running involves predictive maintenance of aging assets, retrofitting of digital monitoring capability, behind-the-meter energy storage to smooth impulsive loads, and the transition toward high-efficiency DC power distribution – where a shift behind the meter can deliver a 10–20 percent efficiency gain.</p>
WHY ASSET STRATEGY IS NOW BUSINESS STRATEGY
Utilities, manufacturers, oil and gas operators, commercial building owners, and data center operators face different operational realities – but the same underlying pressure: aging assets, rising demand intensity, cost exposure, and tightening regulation are converging faster than conventional maintenance and capital replacement cycles can absorb.
Each sector confronts the energy trilemma on its own terms. None is immune to its consequences. Our research shows that waiting for equipment to fail before acting costs up to ten times more than proactive maintenance. Companies that are leading the pack are those shifting from reactive firefighting to structured asset stewardship – treating electrical infrastructure not as a sunk cost, but as a manageable, flexible asset.
THE FUTURE OF ELECTRIFICATION SERVICE: 2026–2035+
<p>A roadmap for achieving operational certainty, energy resilience and business continuity in an increasingly complex energy landscape.</p> <p> </p>