INTRODUCTION

Drive Composer is a start-up and maintenance tool for ABB's common architecture drives. The tool is used to view and set drive parameters, and to monitor and tune process performance. From installation to performance tuning, Drive Composer helps you achieve reliability, efficiency, and peace of mind in every step of your drive lifecycle.

 

Drive Composer 2 – Recommended tool
The full-featured, proven tool for commissioning, configuring, and monitoring ABB drives. Provides the broadest functionality and remains the primary choice for most applications.

 

Drive Composer 3 – Early-stage next generation
Offers a refreshed user experience and supports selected use cases. Still under development with new features added over time. Install alongside Drive Composer 2 and use it when its streamlined workflows fit your needs.

DRIVE COMPOSER USB CONNECTIVITY ISSUE WITH WINDOWS 11

An issue has been identified affecting Drive Composer connectivity after updating Windows 11. Windows 11 update blocks the USB driver due to changes in Windows driver policy enforcement.

For more details, refer to the detailed Product Advisory document.

BENEFITS AND FEATURES OF DRIVE COMPOSER 2

A tool for a drive’s entire life cycle

Drive composer is designed to support the daily operation of ABB drives built on the all-compatible drives architecture, such as ACS880 industrial drives. The tool provides capabilities to view, set, edit, save and back up drive parameters. Diagnostic functionalities help users ensure that drives run reliably and efficiently.

View, set and compare parameters

The parameter window displays the drive’s parameters and signals. Users may view and set parameters and compare changes between the current set and the previous one. Modified values are easy to see with a different background color. One button click filters the whole parameter list and shows only modified values that differ from the drive’s default values.

Custom workspace

Drive composer includes functionality to create own customized parameter windows. User can copy parameters and signals that he/she is interested about to a custom parameter window. There is possibility to create several custom parameter windows for different purposes (IO setup, motor setup, start/ stop, etc.).

  • Online and offline modes available
  • Use the USB port of an Assistant control panel for PC tool communication
  • Use Bluetooth of an Bluetooth Assistant control panels for PC tool communication. This is available in the first phase only for Entry version
  • Use Ethernet-based fieldbus adapter module or Panel bus network connection - Pro version
  • Control, monitor and display status of the connected drive
  • Work simultaneously with multiple drives (networked drives) - Pro version

  • Management of connected drive parameters (Display & modification)
  • Edit parameter files in offline mode - Pro version
  • Copy/download parameters to a drive
  • Customization of parameter windows
  • Save and export parameters to a parameter file
  • Compare parameters between parameter lists or drives - Pro version
  • Drive parameter conversion tool (for ACS800/ACS600) - Pro version
  • User parameter set functionality (only ACS880 drives) - Pro version

  • Monitor signals in numerical and graphical format (Max 8 signals for Entry version and Max 26 signals for Pro version)
  • Monitor signals simultaneously from multiple drives connected - Pro version
  • Save and Export monitored data to a computer
  • Open and analyze the saved or monitored files

  • Adaptive programming feature (Create and edit programs)
  • Control diagrams for parameter setting and diagnostic purposes - Pro version
  • Creation, configuration and execution of Macro scripts - Pro version
  • Configure the optional safety functions modules (FSO) - Pro version
  • Firmware loader (Offline and cloud update drive) - Only offline for Entry version
  • Drive text editor (manage user editable texts in a drive) - Pro version
  • Create EDS export files of a connected drive - Pro version
  • Display contents of an event logger (faults and warnings) - Partly for Entry version
  • Display and analyze of data logged in a drive - Pro version

  • Display of System info (basic information about the drive and its options)
  • Connect to Drive installed base (DIB) service portal (register, search, report)
  • Backup/restore functions
  • Advance restore (restore a set of components/parameter settings) - Pro version
  • Create backup of all connected drives in a computer network - Pro version
  • User interface available in different languages
  • Virtual drive launcher available - Pro version
  • Use an OPC-based commissioning and maintenance tool - Pro version

BENEFITS AND FEATURES OF DRIVE COMPOSER 3

Ease of use

Easy to get started, backwards compatible and future-proof, this all-in-one tool works seamlessly on both PC and mobile devices to accelerate commissioning and minimize risk.

Increase efficiency

With fast connectivity options, quick and effortless commissioning, advanced features for power users, and secure cloud access, the solution is designed to boost productivity at every level.

Improve security

Secure by design, the solution enables reliable remote troubleshooting and delivers smooth, regu-lar application updates for long-term peace of mind.

\

RELATED CONTENT

ABB Drives Software Tools subscriptions

Fast and flexible way to upgrade your drive experience

Virtual drive

Virtual engineering and commissioning allow machine builders and system integrators to develop and simulate entire industrial processing lines and machines, including ABB drives, without actually running the hardware.

Drive IEC programming

Drive application programming allows you to add a competitive advantage to your machines.

Drivetune

Drivetune mobile app is a powerful tool for drive users to manage drives remotely using a smartphone or other mobile device.