BASICS OF THE HARMONICS

Harmonics cause interruptions, interference, and downtime by polluting the electrical network and making connected equipment behave erratically.

 

Harmonics can cause damage to sensitive electronics, interference in communication equipment, and false readings on measurement devices. Harmonics can trip circuit breakers, blow fuses and cause capacitor failures. The effects also include overheating of transformers, cables, motors, generators and capacitors. Equipment must be designed to tolerate harmonics in the network, and oversizing leads to higher investment costs and underutilized capacity.

 

The problems caused by harmonics result in increased losses because more energy is wasted due to overheating, equipment has a shorter life time and is subject to unreliable operation. In the worst cases, harmonics cause unnecessary and unwanted process interruptions.

CAN ABB DRIVES REALLY GET THDI DOWN TO 3%?

That’s the question our customers ask us most often, so we decided to show you the proof. Harmonics can waste energy, damage equipment and cause costly downtime, but ABB’s ultra-low harmonic drives solve the problem without extra filters. In this video our expert explains why harmonics matter, demonstrates how the technology works in practice, and shows live how THDi is reduced to just 3%, helping you protect operations, equipment and efficiency.

WHAT ARE HARMONICS?

In an ideal case, the current in an electrical grid is a pure sine wave and does not contain harmonics. In reality the current deviates from this pure sine wave and contains harmonics. A pure sinusoidal voltage and current does not contain any harmonics Voltage and current that deviate from the sine form contain harmonics The total amount of harmonics is expressed as a THD% value (= total harmonic distortion).

WHAT CAUSES HARMONICS?

Harmonics are introduced into the electrical network by non-linear loads, such as

  • power supplies of PCs, PLCs, TVs etc.
  • photocopiers, domestic appliances
  • diode and thyristor bridges
  • uninterruptible power supplies
  • motor starters
  • switched-mode power supplies
  • variable speed drives

ULTRA-LOW HARMONIC DRIVES BY ABB

ABB has a wide portfolio of industrial and industry-specific ultra-low harmonic drives (ULH) for HVAC, water and wastewater applications based on active front end technology, which offers multiple benefits to industry. Besides harmonics, which are the distortion component of reactive power, ULH drives also take care of the displacement component of reactive power.

Discover insights in a white paper

PREVENTION IS BETTER THAN A CURE FOR THE SYMPTOMS

  • keep the electrical network clean
  • reduce the risk of disturbances
  • prevent damage to other equipment
  • prevent interference with communications equipment
  • reduce the installation footprint
  • reduce the total cost of ownership

Instead of trying to tackle harmonics by often ineffective actions, like adding cooling or over-dimensioning equipment, why not employ equipment that do not cause harmonics in the first place?

LOW HARMONIC CONTENT

ABB's ultra-low harmonic drive produces exceptionally low harmonic content and exceeds requirements set by low harmonic standards. Compared to a conventional drive, the harmonic content is reduced by up to 97%. The total harmonic current distortion is typically 3%. With a passive filter the typical total harmonic distortion is between 5 to 10%.

KEY BENEFITS

Simple and cost-efficient installation

The compact drive features built-in harmonics mitigation. This includes an active supply unit and a low harmonic line filter. As there is no need for external filters, multi-pulse arrangements or special transformers, the simple installation offers significant space, time and cost savings. As there is less risk of overheating with lower harmonic currents, there is no need to over-dimension equipment such as transformers and cables.

Output voltage stabilization for secured operation and optimized dimensioning

The drive’s active supply unit can boost the output voltage to enable full motor voltage, even when the supply voltage is below nominal. This ensures reliable operation in weak networks. This voltage boost capability can also be utilized to overcome voltage drops caused by long supply or motor cables. Therefore there is no need to over-dimension the motor or supply transformer due to long cables. The possibility to stabilize the output voltage of an ultra-low harmonic drive is an advantage compared to passive filter solutions. At nominal loads with a passive filter there is typically a 5% voltage drop. On partial loads on the other hand the voltage over the passive filter can rise by up to 10%, creating the possibility of an overvoltage fault occurring.

Efficient energy utilization

Ultra-low harmonic drives achieve a unity power factor, indicating that electrical energy is being used efficiently. The drive offers the possibility for network power factor correction in order to compensate for the low power factors of equipment connected to the same network. It can help to avoid penalty charges set by electrical utilities for poor power factors. Lower harmonics and full motor voltage at all times mean reduced system losses and better overall system efficiency.

For all industries and applications

Our ACS880 ultra-low harmonic drives are customized to meet the precise needs of most industries, such as the oil and gas, chemical, pulp and paper, food and beverage, rubber and plastics, marine, metals and mining industries. Industry specific ultra-low harmonic drives ACH580 and ACQ580 are available for the HVAC and water industries.

\

PRODUCT OFFERING

ACS880-31 wall-mounted ultra-low harmonic single drives

Everything in one compact wall-mounted ultra-low harmonic single drive to keep your network clean of harmonics.

ACS880-37 cabinet-built ultra-low harmonic single drives

The compact ACS880-37 produces exceptionally low harmonic content in the drives input. By managing and controlling harmonics, the ACS880-37 reaches unity power factor.

ACS880-34 ultra-low harmonic single drive modules

Optimize your cabinet building by managing and controlling harmonics with advanced ultra-low harmonic single drive modules.

ACH580-31 drives

The benefits of a drive without the inconvenience of harmonics.

ACH580-34 drives

Exceptionally low harmonics in high power.

ACQ580-31 drives

Wall-mountable ultra-low harmonic drive.

ACQ580-34 drives

ACQ580-34 offers high power in a compact design with <3% THDi, easy installation, and built-in filters for efficient maintenance and servicing.

\

RELATED CONTENT

Driving down electrical harmonics is key to Google's CDU cooling initiative for AI data centers

Christian Leal, ABB's Global Sales Manager explains why ultra-low harmonic drives are an essential component for any manufacturer with ambitions to pick up Google's Project Deschutes coolant distribution unit baton.

Heidelberg’s municipal utilities rely on ABB ultra-low harmonic drives

With very low harmonics and reliable motor control, ABB boosts efficiency, protects power quality, and delivers dependable low-carbon heat.

Harmonics mitigation technologies

ABB Ultra-Low Harmonic (ULH) Drive

Power quality as leverage in Malaysia's new carbon sensitive landscape

Calefa’s heat pump plants and ABB’s ULH drives improve Orion’s energy efficiency

ABB’s ULH (ultra-low harmonic) drives play a key role in Orion’s heat pump plants in Turku and Espoo, Finland, improving their energy efficiency and ensuring the reliable operation of the plant.

Ultra-low harmonic and regenerative drives for increased efficiency and reliability of processes and systems

Managing and controlling harmonics

Active front end drive technologies

Guide to harmonics with AC drives

Calculate network harmonics with DriveSize