IEC LOW VOLTAGE MOTORS

ABB delivers a comprehensive range of low voltage motors built for exceptional reliability, ruggedness, and efficiency. Designed for all industrial sectors, our motors improve energy performance and productivity while complying with global efficiency standards.

 

ABB low voltage motors operate direct-on-line or with variable speed drives to form optimized motor-drive packages. These systems are engineered to reduce energy use and enhance control across all applications.

 

With over 45% of global electricity consumed by motors and the number of motors expected to double by 2040, energy efficient motors are more critical than ever. Upgrading to ABB’s IE5 Ultra Premium Efficiency motors can cut energy use, lower heat generation, and extend equipment life. Even replacing one motor can make a meaningful impact.

 

Our motors are designed for every industry, offering maximum reliability and long-term performance in the most demanding conditions. Flexible, modular construction allows for easy customization and installation.

IEC LOW VOLTAGE MOTORS, INDUSTRIES AND TOOLS

Products

TITLE

Intro text

\

RELATED CONTENT

Innovative motors offer new opportunities to boost energy efficiency in hazardous areas

Pekka Uusitalo, Global Business Line Manager for IEC Low Voltage Motors at ABB suggests that this is the perfect opportunity for operators to adopt innovative energy-efficient technology that will boost productivity as energy costs soar.

Walking the talk: Inside ABB’s low-carbon motor factories

Stefan Floeck, Division President of IEC Low Voltage Motors, ABB , explains how ABB’s ‘Engineered to Outrun’ philosophy is reshaping its own low voltage motor factories, from zero waste to low‑carbon, renewably powered operations.

LV Titanium VSM delivers IE5 Ultra-Premium efficiency in a compact design

ABB’s LV Titanium Variable Speed Motor (VSM) platform delivers the benefits of an IE5 Ultra-Premium efficiency motor and variable speed drive (VSD) technology in a single, compact, plug-and-play solution.

Why Motor Efficiency Is the New Baseline, Not the Finish Line

ABB is changing the energy efficiency game with its new IE6 synchronous reluctance (SynRM) motor range, bringing hyper‑efficient, magnet‑free performance to key industrial applications.

ABB LV Titanium VSM rewrites the rules of energy efficiency & innovation

Global energy demand shows no sign of slowing down. According to the International Energy Agency (IEA) World Energy Outlook 2025, total demand grew by more than two per cent in 2024 to over 650 exaJoules – well above the long‑term average increase of 1.4 per cent.

ABB IE6 SynRM motors deliver a major boost for industrial energy efficiency

ABB is accelerating industrial energy efficiency with its expanded range of IE6 Hyper‑Efficiency synchronous reluctance (SynRM) motors. This magnet‑free technology—now available from 110 to 450 kW in frame sizes 280 and 315, and speeds up to 3600 rpm.

ABB save 25 GWh of electricity per year for Europe’s leading copper producer

Aurubis’ Pirdop plant in Bulgaria is located around 70 km east of the capital, Sofia. It plays a key role in the Group’s network, processing copper concentrates and producing copper cathodes and anodes, as well as co-products like sulfuric acid and iron silicate.

Power change: Decarbonising Asia by 2026

In Asia, many motors in use are still older IE2 or E3 models, installed decades ago and operating far below today's standards. While 99% of lifetime costs come from the energy they consume, businesses often focus narrowly on purchase price.

How compact variable speed motor systems can unlock energy and emissions savings for water utilities

Pumps, blowers, and aerators are the largest energy consumers within the water sector, accounting for the bulk of operating costs for utilities and municipalities. As energy demand surges, utilities face mounting pressures from both sides: escalating operational costs due to rising electricity prices and increasing scrutiny to reduce their carbon footprint in line with climate targets.

Synchronous Reluctance Motors Can Change the Industry

How synchronous reluctance motors significantly impact energy efficiency while simultaneously reducing operating costs is well known to Stefan Floeck.

Energy efficiency isn't just good for the planet, it's good for business

In ABB's upcoming study, Energy efficiency: the decisive factor, we outline how industries can and must make energy efficiency a priority. It all begins with the electric motor: the beating heart of industrial operations.

New developments in electric motors for the metals industries

The metals industry is at a turning point. With global demand for steel, aluminium, and copper accelerating, producers are facing a critical challenge: how to grow profitably and sustainably in an increasingly competitive market.

ABB accelerates industrial energy efficiency with strategic investment and launch of IE5 motor range in India

Strengthening its footprint, ABB is investing over USD 17 million to expand and modernize its Low Voltage (LV) motors manufacturing facilities in India.

ABB expands IE5 SynRM motor range to enable Ultra-Premium efficiency in more applications than ever

ABB has expanded its IE5 SynRM motor portfolio with three smaller frame sizes (90, 100, 112), now covering 0.75 kW to 450 kW. This gives customers the broadest range of magnet- and rare earth-free motors to boost efficiency, reliability, and sustainability across even more applications.

ABB unifies motor and drive in a streamlined plug-and-play platform

ABB’s new LV Titanium Variable Speed Motor platform delivers the benefits of a high-efficiency motor and variable speed drive (VSD) technology in a single, compact, customizable, plug-and-play solution that enables industrial customers to minimize their energy consumption, save money and reduce carbon emissions.

How ABB’s Low Voltage motors are driving sustainability in the water industry

At the same time, water scarcity, rising energy costs, and sustainability goals are pushing the industry to find more efficient and reliable ways to manage water and wastewater.

Measuring motor energy efficiency - From manufacturing to operation

In industry, there is often a perception that sustainability and profitability are in conflict. When it comes to industrial electric motors, however, energy efficiency allows both objectives to be achieved at the same time.

ABB Motors & Generators China Celebrates Anniversaries with Energy Efficiency Milestone

On April 8, ABB Motors & Generators China marked its significant anniversary milestone by hosting a media open day at the Shanghai site, celebrating 30 years of IEC low-voltage motors, and 20 years of large motors and generators manufactured in China.

ABB General Performance motors - the EU’s ‘right now’ choice

Energy efficiency is a key priority for the EU Clean Industrial Deal, especially when it comes to the millions of industrial electric motors that power industrial applications such as fans, pumps and compressors.

Boosting productivity in the metals industry with IEC low voltage motors

Rapidly increasing demand for steel, aluminium, and copper has brought the metals industry to a critical juncture, and ensuring that growth is sustainable globally is an ongoing challenge.

News, customer cases and press releases

Discover our latest customer cases, success stories, and news to learn how at ABB we help industries run leaner and cleaner.

Manuals for IEC Low voltage motors

Looking for a manual for your IEC low voltage motor?

DISCOVER YOUR MOTOR SOLUTION

  1. Find the right motor & drive

    Search our comprehensive list of motors and gain access to detailed product specifications, technical data, and product documentation.

  2. Contact us or find a partner

    Our global network of salespeople and channel partners is dedicated to supporting you with your application wherever you are in the world.

  3. Our expertise at your service

    ABB Motion Services helps you maximize uptime, extend product lifetime, enhance performance and boost energy efficiency of your motors, generators and drives.

EXPERTISE AND TECHNOLOGY

ABB EcoSolutions

ABB EcoSolutions provides enhanced transparency on the environmental impact across product lifecycle from inception through to disposal. Designed for high recyclability and manufactured with sustainably sourced materials. Made with processes that are designed to avoid waste. Designed to increase resource and process efficiency while in use, be upgradable and optimize the lifetime of equipment and facilities. Provided with instructions for responsible end-life treatment.

IE6 hyper-efficiency with SynRM magnet-free motors

Well-proven synchronous reluctance motor (SynRM) technology is first magnet-free design to reach IE6 hyper-efficiency - an anticipated efficiency level ABB defines as achieving a 20 percent reduction in energy losses against comparable IE5 motors. Early adopters of IE6 hyper-efficiency motors will reap the benefits of reduced energy costs and increased productivity while moving ahead of current sustainability targets.

Ecodesign directive

There is rapidly growing demand worldwide for more efficient products to cut energy consumption, reduce emissions and help to build a more sustainable future.

Energy efficiency

Nearly 70 percent of all electrical energy in industry is used to power motors. They enable applications to run in an industry process, such as pumps moving liquids, or fans moving air. Lowering CO₂ emissions and increasing energy efficiency is critical for our planet, but also for ensuring stable and productive industry operations.

Efficiency calculator

Calculate the potential monetary savings and ROI by upgrading to a more efficient motor. By entering details like voltage, speed IE Class, it will estimate potential savings and payback time, helping you assess the value of the upgrade.

Motion services

ABB Motion Services helps you maximize uptime, extend product lifetime, enhance performance and boost energy efficiency of your motors, generators and drives. Our tailored services and digital solutions keep your operations running profitably, safely and reliably.

ABB Drives

ABB Drives is a global technology leader serving industries, infrastructure and machine builders with world-class variable speed drives, drive systems and packages. We help our customers, partners and equipment manufacturers to improve energy efficiency, asset reliability, productivity, safety and performance.