MAKES YOUR ROBOT WELDING MORE EFFECTIVE AND ACCURATE
Robot welding stations are today a common and well known tool in the industry. The continuous development of robots, welding equipment and work piece positioners has dramatically decreased the cycle time and increased the uptime.
The worst load in a robot welding cell has the welding torch. It is exposed for heat, welding spatter and in worst case, collisions. Welding torches are made for such environment but need regularly cleaning, measuring and TCP-definition in order to weld with good quality and accuracy. It consists of three main units – a mechanical torch cleaner, a tool center point definer and a wire cutter.
Regular TCP confirmation is necessary because there are a number of things that can cause the welding torch to be out-of-position:
- A collision with the work piece, e.g. the robot hitting a fixture clamp which was left in the wrong position.
- Incorrect defined TCP.
- After exchange of the welding torch.
- After exchange of the swan neck.
FULLY AUTOMATED TOOL CENTER POINT PRECISION
During the setup of the robot station, the Torch Service Center (TSC 2013) automatically determines the Tool Center Point (TCP).
Once production is running, the robot can be programmed to visit the TSC at regular intervals to check the TCP, make any necessary adjustments automatically, and then return to work with perfect precision.
The integrated wire cutter ensures an exact and consistent wire stick-out length. This precision allows the TSC 2013 to define the TCP right to the tip of the wire and at the exact center of its diameter—ensuring consistent, high-quality welds every time.
KEY BENEFITS
Better up-time
Better up-time in the robot station, giving more production hours.Improved welding quality
Improved welding quality, resulting in reduced repair cost to almost zero.Trust
Customers can trust the TCP in their robot system, they faster locate other tolerance problems in their own part production.TECHNICAL DATA