ArcSave: Revolutionizing Electric Arc Furnace Steelmaking

In the fiery heat of a steelmaking furnace, molten metal is being stirred. It is stirred steadily, as if by an unseen hand, assuring the homogeneity of the molten steel. This contactless electromagnetic stirrer, invented by ABB, is introducing new levels of precision and energy efficiency to the steel industry. Meet ArcSave.

news

2min

2025-11-20

Steelmaking in electric arc furnaces (EAFs) involves melting the metal using high-voltage electric arcs. If molten steel is not stirred, it develops inconsistencies in temperature and chemical composition. Metal can solidify at the bottom of furnace forming what steelmakers call the “skull”. These effects degrade product quality and increase energy consumption.

 

Stirring solves these problems by ensuring that heat and alloying elements are distributed evenly throughout the melt, improving homogeneity and accelerating scrap dissolution. 

 

In some furnaces, stirring is mechanical or gas-based, but these methods have limitations in control, efficiency, and maintenance. Electromagnetic stirring (EMS) was invented in 1937 in Sweden by Dr. Ludwig Dreyfus of ABB’s predecessor company, ASEA. The method is suited for conductive molten materials such as steel, aluminum, and copper. The latest version of this stirrer, ArcSave, pushes the advantages to higher levels.

 

ABB’s electromagnetic stirrers are essentially huge electromagnets placed beneath the furnace. The physical principle is pretty much the same as for an electric motor. Fixed electromagnets create moving magnetic fields that in turn induce currents and electromagnetic forces inside the molten steel – and keeps the melt moving. This approach is non-invasive, powerful, and controllable.

ABB ArcSave is being installed on Turkish steelmaker Colakoglu Metalurji’s jumbo 370-tonne capacity EAF - the largest of its kind in the country. Image: Colakoglu Metalurji

THE LOW-CARBON ADVANTAGE

One of the most compelling benefits of EMS is its contribution to decarbonization. Steelmaking is traditionally carbon-intensive, but EMS helps reduce emissions in several ways:

Energy efficiency

By improving heat transfer and reducing power usage, EMS cuts overall electricity consumption.

Reduced electrode use

EMS stabilizes the electric arc, minimizing fluctuations that wear down graphite electrodes. Since electrode production and use are carbon-intensive, reducing their consumption lowers the overall carbon footprint.

Less re-melting and waste

Stirring prevents the formation of bottom skulls - solidified metal that must be re-melted. Avoiding this waste improves material efficiency and reduces the energy needed for reprocessing.

Optimized scrap use

EMS enables the use of larger and more varied scrap charges, reducing reliance on virgin iron sources like pig iron or direct reduced iron, which are more carbon-intensive to produce.

ArcSave electromagnetic stirring rapidly homogenizes temperature distribution and chemical composition in the EAF melt while speeding up scrap and ferroalloy melting.

ARCSAVE

Key facts about ABB’s ArcSave:

+5–7%

Productivity

-3–5%

Total energy consumption

-5–7%

Power-on time

+1%

Iron yield

Lower...

...alloy, lime, electrode and refractory consumption

Stirring ahead

An onboard battery can be used as the main energy source in battery electric vehicles and enable them to operate over non-electrified sections. In hybrid vehicles, the battery works as a buffer storage and provides peak power that helps to reduce the installed power of the primary power source, be it the diesel engine or a fuel cell, and allows the recuperation of braking energy. Further, peak shaving helps to operate the primary power source more often at its maximum efficiency point and reduce fuel consumption.

STAY AHEAD IN INNOVATION & TECHNOLOGY

Get our latest news, insights, and breakthroughs straight to your inbox.