ABB’s solutions for plant-wide planning, management and monitoring of the newspaper production process give printing houses the means to achieve an overall optimization of their production at one or more printing site.

OUR SOLUTIONS

MPS Cockpit

MPS COCKPIT

<p><b>Managing and optimizing the entire newspaper production process</b></p> <p>MPS Cockpit is a planning, management and monitoring system for the entire newspaper production process from product definition to delivery across one or more printing sites.</p> <p>MPS Cockpit applies the principles of lean manufacturing and optimizes the planning process by starting with the definition of the final product as delivered to the readers. Then the planning of its production is made. MPS Cockpit’s efficient use of planning templates means that a year’s production of a newspaper can be planned in two minutes with the possibility of adding further detail and precision at later dates.</p> <p>The main advantages are immediately clear. There is a clear overview of the product and its production, and the production plans in the various departments are completely consistent. Planning conflicts and the resulting costs are avoided.</p> <p>When the time for production comes, MPS Cockpit distributes the orders and planning data to the individual subprocesses such as the press and the mailroom.</p> <p>The central position of MPS Cockpit, its interfaces to the production management systems of the individual subprocesses and the addition of copy counters at strategic points in the plant also make it a tool for monitoring the progress of the productions.</p> <p>The integration with distribution, subscriber and other commercial systems opens a wide range of further possibilities for improving efficiency and reducing costs. MPS Cockpit takes newspaper production to a new level of automation.</p>

Planning

<p>Planning, management and monitoring of the entire production process from a single workplace</p>

Output

<p>Allows the planning of the final product as delivered to the readers, including inserts</p>

Templates

<p>The use of templates means that a year’s production can be planned in minutes</p>

Capacity visibility

<p>Makes free production capacity visible across the entire process</p>

Full functionality

<p>Full functionality with one or more printing sites</p>

Interfaces

<p>Extensive optional interfaces couple commercial systems with production management</p>

MPS INSIGHT

<p><b>Plant-wide production reporting and analysis</b></p> <p> </p> <p> </p> <p>In order to improve an industrial process and the resulting profitability it is first necessary to know where one is starting from. For the newspaper production process at one or more sites the ideal tool for this is MPS Insight. The core of the system is the data warehouse, which provides long-term storage of all relevant production data. This serves as a priceless source of data for generating both standard and user-specific reports.</p> <p>&nbsp;</p>

Browser-based system

<p>Browser-based system: reports available anywhere to authorized users</p>

Reporting and analysis

<p>Reporting and analysis of individual subprocesses and across the whole production process</p>

Subscription system

<p>Subscription system for the automatic e-mail distribution of reports to users at specified times</p>

Central, fully documented database

<p>Central, fully documented database for the storage of all process values. Data available for other applications</p>