Overview

When St. Croix Tissue opened their greenfield site in the eastern U.S. with annual production capacity of 120,000 tons, there were many operational areas to shape as production took off. 

 

With ABB Ability™ Manufacturing Execution System (MES) for pulp and paper, the mill gained the flexibility needed to manage evolving operations from day one.

CASE STUDY DATA

Industry

Pulp and Paper

Customer

St. Croix Tissue

Location

Baileyville, Maine, USA

The Situation

  • Greenfield site

  • Concurrently implementing the system, building machines and infrastructure

The Solution

Benefits

  • Efficient end-to-end management 
  • Transparency for optimized productivity
  • Improved quality and customer satisfaction

 

An implementation to gain flexibility during changes

For the mill being launched by St. Croix in Baileyville, Maine, the decision was made to capitalize on synergies and implement ABB Ability™ MES, since ABB was the automation and quality control supplier.

 

“One thing we liked about ABB’s system was that it was end-to-end,” said Nellie-Jo Lee, Senior Systems Analyst and SQL Database Administrator, St Croix Tissue. “We understood you could do certain modules, but we wanted something that covered one end to the other.”

 

The mill was a greenfield site and had to balance implementing the system, building machines and infrastructure, and executing multiple start-ups. Yet they achieved a unique-to-the-MES-industry status when the mill went live on its own without the need for on-site support, as is typically required for MES implementations.

 

“The ABB team gave us all the tools we needed,” said Lee. “We were very flexible to get everything up and running the way we did. And ABB was great helping us because it took a while for everything in the mill to be fully operational.”

 

This included train-the-trainer sessions and refresher training as needed. Plus, the team benefited from Lee’s own experience with these type of systems, becoming the on-site, go-to person for all things MES.
 

Efficient end-to-end management

Once the mill was fully operational, they could take advantage of the full suite of MES modules, which covers the whole order-to-cash process and beyond. Production can be planned to help align order intake with the most efficient use of personnel time, raw material, and resources to meet their end customer delivery and quality expectations, while providing the mill the efficiency and transparency needed to optimize production.
 

“From my perspective, it seems very thorough,” said Jesse Stephens, Operations Manager, St. Croix Tissue. “When I’m wishing I had some system in place, there is usually a feature already in ABB’s MES that we just haven’t realized was there. We couldn’t run the business without it.” 

 

There’s also the matter of making day-to-day operations easier. For instance, the mill finds value in the ability to email delivery notes, packing lists, invoices, and more from the system itself.

 

“Other systems ‘automatic email function’ is not automatic,” said Lee. “With ABB, we can reduce steps with the built-in feature and configure it for different user needs, getting information to target in a more timely fashion.”
 

Finding new opportunities in what’s available

The system offers so many valuable features, it can take time and specific circumstances to uncover new helpful aspects.

 

Features within the Quality Data Management module is one example. Previous mill personnel had been beholden to excel-based complaint tracking. When Stephens came into the position, Lee helped augment the approach by pointing out the available features in MES.

 

“The quality system helps with data gathering and analyzing to track complaints better,” said Stephens. “We can use our own business objectives to create any type of reporting structure, and it sets us up to have the data we need to make improvements.”
 

Flexibility for changing operations

Key for the mill is the ability to easily make changes in the system based on what operations currently demands.

 

“One of the reasons we purchased ABB was because of the ability to configure a lot of different functions without requiring a program change,” said Lee.

 

For example, working to incorporate a buy-back process when converted goods come back to the mill to sell direct. And when new warehousing options needed to be added to the system. Or accommodating new roll size changes. Or when the business model transformed.

 

Changes can be made by the St. Croix team and ones that require support are covered under hours available in their ABB service agreement.

 

“ABB has been easy to work with and very accommodating,” said Lee. “And if you make a simple request, the whole process is simple. They don’t overcomplicate small matters and that’s really appreciated as well.”
 

A system made for pulp and paper

One of the things that stood out to Stephens was the specificity of which to keep track of and manage different grade and end customer requirements, something critically important to tissue, board and papermakers’ end product profitability.

 

“The system has a structure there to keep all unique properties assigned to a customer. From a quality specs standpoint, I can also have specifics in the system and product defaults,” said Stephens. “Having a space to keep track of all those different grades is really helpful.”

 

Lee, Richards, and Stephens would recommend ABB’s MES to other mills. “One of the driving factors in the initial decision was the ability to interface with the quality and automation systems also from ABB,” said Richards. “That has lived up to our expectations and support our decision to go in that direction.”

ABB’s MES suite covers the whole order-to-cash process (red lines) and beyond, providing modules that also optimize the product value chain (grey lines)

WHAT OUR CUSTOMERS SAY

“In our evaluation of suppliers, ABB offered more flexibility around changes. ABB’s system could accommodate simple changes without significant cost increase.”

Marty Richard, Mill Manager, St. Croix Tissue

“We couldn’t run the business without it.”

Jesse Stephens, Operations Manager, St. Croix Tiss

“There’s a lot more that we can do and will be doing in the future to help run the business better or smarter.”

Nellie-Jo Lee, Senior Systems Analyst and SQL Data

"The ability to interface with the quality and automation systems also from ABB has lived up to our expectations and support our decision to go in that direction.”

Marty Richards, Mill Manager

\

RELATED LINKS

ABB Ability™ Manufacturing Execution System for Pulp and Paper

ABB provides the operational foundation for the next generation of pulp and paper optimization with a comprehensive order-to-invoice solution designed to meet and grow with your business.

Digital applications for pulp and paper

ABB supplies advanced industry-specific software and services that enable modern pulp & paper mills to maximize visibility, reliability, productivity and energy efficiency and optimize performance across the enterprise

Digital transformation in the pulp and paper industry

Our digital experts know what it takes to make quality paper. That’s because their expertise is grounded in the day-to-day realities of the mill.

Data management: the formula for pulp and paper analytics success

Effective data management requires having a strategy and reliable methods to access, integrate, cleanse, govern, store and model - to prepare data for analytics so that it adds value.

ABB delivers integrated systems for St. Croix Tissue

Integrated electrical and automation systems, equipment and services for St. Croix Tissue; single operations environment provides highest level of efficiency, reliability and product quality.