ABB Ability™ Plant Optimizer for pulp mills enables real-time pulp tracking with synchronized setpoint management that eliminates timing errors during grade transitions - preventing chemicals overdosing and off-spec production.

From Manual Coordination to Precision Timing  

A major European kraft pulp mill produces 15 distinct pulp grades, each with up to 20 unique recipe parameters. The fiber line includes continuous digesters feeding into a 3-stage bleaching sequence with dedicated storage tanks for on-spec and off-spec material.

 

For years, grade transitions were managed manually. Operators would receive static time estimates and adjust recipe parameters - temperature, chemical dosages, steam flow, wash liquor composition - at predetermined intervals. With each bleaching stage having a different residence time, and without knowing exactly where the grade boundary actually was in the process, operators faced an impossible choice:

  • Make conservative adjustments and extend the transition, wasting chemicals and production time
  • Make aggressive adjustments and create off-spec material that had to be rerouted to recovery tanks
  • Manually monitor output quality and react too late

This unpredictable "twilight zone" - the period when pulp properties were transitioning - created both operational risk and cost. Off-spec production was the hidden tax of grade complexity. 

 

How do you predict when a grade front - which doesn't move as a sharp boundary but as a blurred, mixing zone - will reach each critical process point, accounting for variable flow rates, non-ideal mixing in reactors, and residence time variability? The answer required validating that predictive models could match reality. And it had to work in a live mill running multiple shifts, with real market pressures.

The Twilight Zone Decoded: Predicting Grade Boundaries Within Minutes  

 

ABB deployed an end-to-end tracking system that operates as a coordinating layer on top of the existing DCS infrastructure. The system works in three stages:

 

1. Real-time pulp monitoring - As the new grade enters the fiber line, the system continuously tracks its position through mass and component balance calculations and residence time distribution (RTD) modeling. The tracker knows:

  • Exactly how long pulp stays in each reactor
  • How properties evolve (kappa number, brightness, pH) as the grade moves downstream
  • The predicted "twilight zone" window where on-spec and off-spec material are mixed

2. Predictive notifications - Using these calculations, the system predicts precisely when the grade boundary will reach each critical process point (digester discharge, OP1 inlet, D/Q2 inlet, OP2 inlet, final storage). Two-stage alerts give operators advance warning and time to verify setpoints.

 

3. Synchronized adjustments - As the grade front arrives at each stage, the system can either:

  • Suggest setpoint targets for operator confirmation (assisted mode)
  • Automatically implement setpoint changes based on grade position (automatic mode)
  • Route off-spec material detected in the "twilight zone" to transition tanks 

Orchestrating 15 Grades Across Coordinated Bleaching Reactors

 

The system was rigorously validated against measured retention times across all three bleaching stages. It predicts process timing within customer-specified acceptable control limits. Operators can reliably make synchronized setpoint changes across all three reactors based on these predictions, knowing the margin of error is minutes, not hours. These numbers matter because transition timing is everything - a prediction error means either premature or delayed setpoint changes, both creating off-spec material. 

RETENTION TIME VALIDATION

Alkaline Extraction

  • Actual measured: 1 hr 53 min
  • System predicted: 1 hr 44 min
  • Deviation: –9 min
  • Accuracy: 99.2%

Delignification

  • Actual measured: 57 min
  • System predicted: 57 min
  • Deviation: 0 min
  • Accuracy: 100%

Final Bleaching

  • Actual measured: 2 hr 00 min
  • System predicted: 2 hr 11 min
  • Deviation: +11 min
  • Accuracy: 99.1%

Retention time verification: OP1 and D/Q2 bleaching stages

Benefits of data-driven, Coordinated grade change 

 

This European mill represented the technical frontier - a high-complexity, high-frequency production schedule with digesters, shared buffer systems, and stringent quality requirements. Success here proved that intelligent grade transition management works in real, demanding conditions, with many operational benefits:

  • Precisely coordinated transition timing - from unpredictable hours to measured transitions with automated alerts at each stage
  • Dramatically reduced off-spec production - by eliminating timing errors; off-spec material automatically rerouted to transition tanks
  • Reduced chemical consumption - precise setpoint timing prevents overdosing / underdosing thus avoiding timing uncertainty
  • Significantly improved operator response time - operators confirm recommended setpoints rather than estimating them
  • Grade complexity now manageable - 15 grades × 20 parameters each no longer represents operational risk
  • Fiber line traceability for the first time - complete visibility from digester discharge through final HD storage 
  • Process stability - helps to achieve product quality meeting the specification across all bleaching stages

 

The validated retention time predictions were the key: once operators could trust that the system knew exactly when each stage transition would occur, they could confidently automate the adjustments. This is now the blueprint for other complex mills facing similar grade management challenges.