ABB Ability™ Plant Optimizer for pulp mills enables real-time pulp tracking with synchronized setpoint management that eliminates timing errors during complex grade transitions across cooking, washing, and bleaching. This data-driven approach gives the mill end-to-end intelligence - connecting grade management, recipe control, process tracking, and quality monitoring into a single solution.

Managing grade complexity from cooking to final storage  

At a South African pulp mill producing multiple grades, grade management was a coordination problem that spanned the entire fiber line. Unlike a single-stage quality challenge, every finished pulp grade at this mill was the result of sequential intermediate grades - across cooking, washing, and bleaching - all of which had to be tracked, managed, and transitioned in coordination.

 

The fiber line moves pulp from wood chip blending in the digester, through washing and oxygen delignification, into a multi-stage bleaching sequence - D0, EOP, D1 - and finally into High Density (HD) storage. At a production rate of 760 tonnes per day, even small timing errors in grade transitions translate directly into tons of off-spec pulp and wasted chemicals.

 

Managing this complexity required not just accurate tracking, but a complete, real-time picture of every grade in production simultaneously - its recipe configuration, its position in the fiber line, how much had been produced, and how far it was from its production target.

 

No such unified view existed before this implementation. Process delays, varying flow rates, inconsistencies in tower levels, and non-ideal mixing in blow tanks and reactors all meant that static time estimates were not accurate. Operators responded reactively, adjusting setpoints after quality deviations showed up in lab samples - samples that could be 30 to 60 minutes old by the time they reached the control room.

 

A Unified grade and recipe VIEW

ABB deployed its coordinated grade change system to give the mill end-to-end intelligence across cooking, washing, and bleaching. Every finished pulp grade is mapped to its intermediate grades and associated recipes across all process sections. For each intermediate grade, operators can see - from a single screen - the target setpoint, active setpoint, engineering units, alarm limits, and the specific workplace the parameter applies to. There is no longer any ambiguity about what the process should be doing at any point in a transition.

Predictive grade front tracking through the bleach plant

 

As a new grade moves through oxygen delignification and approaches the bleaching section, the system uses residence time distribution (RTD) models, unit-specific holdup volumes, and consistency-corrected volumetric flows to calculate exactly where the grade boundary is. Rather than providing a single estimated arrival time, the system forecasts the 10%, 50%, and 90% arrival quantiles for each stage - giving operators a statistically grounded window. Every bleaching unit is tracked individually.

real-time Alerts and setpoint updates 

When the system detects that the incoming grade front is approaching a bleaching stage, it automatically generates an alert. This alert displays the grade identifier, the estimated time to arrival, and presents the operator with three choices: acknowledge, ignore, or update setpoints immediately.

 

One of the most operationally valuable features of the system is its continuous on-spec/off-spec quality alerting. Rather than waiting for a lab report to confirm a quality deviation, the system monitors key process indicators in real time and immediately flags when values fall outside specification. 

 

These alerts pinpoint exactly which unit is producing off-spec material, allowing operators to respond immediately - before the deviation propagates downstream and affects final product quality. This shift from reactive to proactive quality management is one of the most significant operational changes the system enables.

Benefits of data-driven, Coordinated grade change 

 

The South African implementation demonstrates the power of intelligent grade transition management in both timing accuracy and operational transparency. When every operator, process engineer, and shift supervisor can see the same live picture of where every grade is, how much has been produced, and what the process is doing right now, decision-making improves at every level:

  • Precisely coordinated transition timing - from unpredictable hours to measured transitions with automated alerts at each stage
  • Dramatically reduced off-spec production - by eliminating timing errors; off-spec material rerouted to transition tanks
  • Reduced chemical consumption - precise setpoint timing prevents overdosing / underdosing this avoiding timing uncertainty 
  • Significantly improved operator response time - operators confirm recommended setpoints rather than estimating them
  • Reduced operator workload - automated alerts replace manual coordination between control room, lab, and shift supervisors
  • Grade complexity now manageable - all active grades, intermediate products, recipes, and production targets on one screen
  • Fiber line traceability for the first time - grade visibility across cooking, washing, and bleaching

Now, the mill anticipates grade changes, manages them proactively, and maintains a continuous, auditable record of every transition across the entire fiber line. This data-driven approach is not only achievable but essential for mills operating in a competitive and more frequent grade-change environment. 

 

The reduction in off-spec pulp, in consumption of chemicals, liquors and  steam suggests that the cost of implementing ABB's pulp tracking system can be recovered within a short operational timeframe.