ABB expands MegaFlex DPA UPS range for Next-Gen data centers

Press release

  • Modular UPS system from 1000 kW to 2000 kW designed for hyperscale, colocation, and neocloud data centers
  • AI-ready power protection with best-in-class VFI efficiency up to 97.6%
  • Universal voltage compatibility (380V–480V) and scalable architecture for global deployment

ABB has launched the MegaFlex DPA UPS system, now delivering from 1000 kW to 2000 kW of intelligent power protection for the world's most demanding data center environments. Optimized for colocation, hyperscale, and neocloud facilities, the MegaFlex DPA brings intelligent energy infrastructure to next-generation data centers. 

“From source to rack, ABB innovations support the rapid expansion and evolution of digital infrastructure for AI workloads,” said Sébastien Surply, Head of Critical Power, ABB Electrification. "This latest addition to our UPS portfolio, enhances the MegaFlex DPA’s AI-readiness. Its modular design makes it ideal for data centers seeking scalable, ultra-high efficiency power protection, and with universal voltage support and a 15-year design life, MegaFlex DPA is engineered for global reach and long-term resilience." 

Designed to meet the exponential growth of AI workloads and real-time data processing, the MegaFlex DPA offers best-in-class VFI efficiency up to 97.6%, a modular architecture for seamless scalability, and true front access for simplified serviceability. The system supports both distributed static and central static internal bypass architecture options, allowing configurations tailored to universal voltages—380/400/415/440/460/480 V, 50/60 Hz, with 3-wire or 4-wire connection flexibility—targeting IT, AI, and mechanical loads. 

ABB has launched the MegaFlex DPA UPS system, now delivering from 1000 kW to 2000 kW of intelligent power protection for the world's most demanding data center environments.
ABB has launched the MegaFlex DPA UPS system, now delivering from 1000 kW to 2000 kW of intelligent power protection for the world's most demanding data center environments.
center

The system’s Xtra VFI mode dynamically adjusts active modules based on load, minimizing energy waste and reducing CO₂ emissions. Integrated with ABB’s SmartTracker platform, MegaFlex DPA benefits from continuous remote monitoring and predictive maintenance insights that help operators maximize uptime, maintain peak efficiency, and extend system life across single‑site and global deployments. 

As AI reshapes our digital world, ABB helps data centers outrun—delivering solutions that combine performance, sustainability, and future-ready design. 

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com 

ABB Electrification is a global technology leader enabling the efficient and reliable distribution of electricity from source to socket. With more than 50,000 employees across 100 countries, we collaborate with our customers and partners to solve the world’s greatest challenges in electrical distribution and energy management. As the energy transition accelerates and electricity demands grow, we are electrifying the world in a safe, smart and sustainable way. At ABB, we are ‘Engineered to Outrun’, and we are passionate about helping our customers and partners do the same. www.go.abb/electrification

  1. Communications Leader, Smart Power

    Email: Sarah.Lippincott@us.abb.com