ABB Robotics’ Flexley® Mover P603 wins iF Design Award 2026
Press release
- iF Design Award given for innovative design and intelligent navigation capabilities
- Highlights ABB Robotics’ focus on delivering adaptable autonomous versatile robotic (AVRTM) solutions for modern manufacturing and logistics applications
ABB Robotics’ Flexley® Mover P603 autonomous mobile robot (AMR) has won the iF Design Award 2026 in the Industry, Tools and Machinery Product Design category, based on its compact design, intelligent navigation and potential to transform performance in intralogistics applications.
“The Flexley® Mover P603 is the latest step in ABB Robotics’ approach to autonomous, software-driven intralogistics automation, where machines can operate independently while working seamlessly alongside people and other systems,” said Alfonso González, Global AMR Product Line Manager of ABB Robotics. “This award recognizes not only the strength of the design, but also how we’re lowering the barriers to automation through more autonomous and versatile robotics (AVRTM) that can do more things, in more places, and do it faster, safer and smarter.”

The P603 was selected by judges for its combination of smart engineering, intelligent software and autonomous functionality in a single solution. Its navigation system, AI-powered by ABB Robotics’ Visual SLAM technology, enables precise movement without the need for fixed infrastructure, which speeds up commissioning by up 20%, compared to other navigation systems, and makes it less complex.
A compact footprint allows it to operate efficiently in space-constrained environments, while integrated load sensing ensures the safe handling of loads of up to 1500 kg. Together, these capabilities give manufacturers a versatile, future-ready solution that streamlines material flow and supports rapid adaptation to changing production needs.
Introduced in 2025, the Flexley® Mover P603 is designed to boost output and improve material flow while reducing setup time and infrastructure requirements. Its quick installation and ability to operate in dynamic environments make it well suited to facilities looking to modernize operations without disruption.
Further information about the Flexley® Mover P603 is available on the official iF Design website under “Winners & iF Ranking”.
ABB Robotics as one of the world’s leading robotics companies, is the only company with a comprehensive and integrated AI-powered portfolio covering robots, cobots and Autonomous Mobile Robots (AMRs), designed and orchestrated by our value-creating software. We help companies of all sizes and sectors - from automotive to electronics and logistics – to outperform by becoming more resilient, flexible and efficient. ABB Robotics is at the forefront of developing and commercializing a new generation of Autonomous Versatile Robotics (AVR), leading a global innovation ecosystem of partners in advancing efficient hardware and intelligent software with industrial performance. The business employs approximately 7,000 people. go.abb/robotics
About the iF DESIGN AWARD
Since 1954, the iF DESIGN AWARD has been a globally recognized benchmark of design excellence. The iF Design brand is internationally established as a symbol of outstanding design achievement, with the iF DESIGN AWARD regarded as one of the most important design honors in the world. It honors design achievements in all disciplines: product, packaging, branding & communication, service design, architecture and interior architecture, user experience (UX), user interface (UI) and concepts. All award-winning entries are presented on ifdesign.com.