ABB Robotics brings industrial-grade physical AI to fashion logistics

Press releases

  • ABB Robotics introduces its first end-to-end vision-based industrial-grade physical AI solution 
  • Fashion Inductor functional module upgraded with AI Robot Trainer, making advanced AI easier to deploy, operate and optimize without needing specialist expertise 
  • Reduces engineering and commissioning effort by up to 75%, enabling system integrators to deploy and scale AI-powered fashion logistics applications faster and with less risk  

ABB Robotics has launched its first end-to-end vision-based industrial-grade physical AI solution, integrating AI Robot Trainer into its Fashion Inductor module to help system integrators deploy, scale and continuously optimize AI-powered fashion logistics applications with significantly reduced effort and risk.  

“Physical AI fundamentally changes what robots can do in industrial applications," said Craig McDonnell, Managing Director, Business Line Industries, ABB Robotics. "Some of the greatest opportunities for physical AI are in applications that have traditionally been difficult to automate because of high variability. Fashion Inductor with AI Robot Trainer is our first end-to-end vision-based physical AI solution, demonstrating how intelligent automation can be deployed, operated and continuously optimized at industrial scale, helping system integrators accelerate deployment, reduce project risk and maintain performance over time.” 

Designed to meet the extreme variability of fashion and apparel logistics, where products, packaging and operating conditions change continuously, Fashion Inductor already delivers high-performance sorting for real-world logistics environments, with throughput of up to 1,300 items per hour per cell and picking accuracy targets above 99.5%, enabled by ABB Robotics' AI-powered Automatic Path Planning, motion accuracy and application-specific vision technology.

The addition of AI Robot Trainer introduces vision-based physical AI capabilities that reduce engineering and commissioning effort by up to 75%, providing pre-trained, fashion-specific AI vision models, application-specific tools and rapid retraining capabilities that help system integrators deploy, adapt and continuously optimize applications as requirements evolve, without specialist AI expertise. 

The upgraded Fashion Inductor also introduces a new digital twin, an exact replica of the module software, connecting Application Controller Platform, Automatic Path Planning, AI Robot Trainer and RobotStudio®. This accelerates commissioning and gives greater flexibility in set-up, including the ability to integrate third-party components such as grippers.  

AI models are not only developed, but continually improved throughout the system lifecycle, against real performance targets and changing operating conditions. AI Robot Trainer enables structured, rapid cell‑specific retraining through a continuous closed-loop workflow that monitors robot performance, identifies anomalies, generates new model training data and deploys improvements back to the physical robot.  

The lifecycle is anchored in ABB Robotics’ core platforms, with RobotStudio providing the foundation for virtual design, simulation, and validation, and the OmniCore™ robot controller serving as the execution layer in production. 

Fashion Inductor marks the first step in ABB Robotics’ broader rollout of vision-based physical AI, a core part of developing more autonomous and versatile robotics (AVR™). The same AI Robot Trainer-powered approach will continue to expand across additional ABB Robotics vision-based applications through Q1 2027, bringing adaptive, lifecycle-managed intelligence to the next generation of increasingly autonomous robotic systems. 


ABB Robotics as one of the world’s leading robotics companies, is the only company with a comprehensive and integrated AI-powered portfolio covering robots, cobots and Autonomous Mobile Robots (AMRs), designed and orchestrated by our value-creating software. We help companies of all sizes and sectors - from automotive to electronics and logistics – to outperform by becoming more resilient, flexible and efficient. ABB Robotics is at the forefront of developing and commercializing a new generation of Autonomous Versatile Robotics (AVR), leading a global innovation ecosystem of partners in advancing efficient hardware and intelligent software with industrial performance. The business employs approximately 7,000 people. go.abb/robotics   

Related Links

Fashion Inductor

  1. ABB Robotics Global Media Relations

    Email: rory.smith@gb.abb.com

    Phone: +447548780120