ABB Robotics launches high-speed PoWa™ cobot family
Press release
- New, high-speed, higher payload PoWa cobot family meets need for industrial-grade performance in collaborative robotics, lowering the barrier to automation for both SMEs and large enterprises
- Payloads from 7kg to 30kg, best-in-class top speed of 5.8 m/s, longest reach and highest arm load on the market
- Powered by ABB OmniCoreTM controller platform and seamlessly integrated with ABB Robotics’ suite of software tools
ABB Robotics is combining the flexibility of cobots with higher payloads and performance, with the launch of its new PoWa cobot family into the rapidly expanding global collaborative robot market, which ABB Robotics estimates will grow by 20 percent annually through to 2028.
“Cobots are growing significantly faster than traditional industrial robots, driven by demands from both small and midsized companies starting their automation journey as well as large enterprises,” said Andrea Cassoni, Head of Collaborative Robots at ABB Robotics. “These customers are seeking higher speeds and payloads, but also greater ease of use, and compact designs. Established manufacturers want to automate heavier, fast cycle applications, without the complexity and operational rigidity of traditional industrial robots. We are meeting these needs with the global launch of our high-speed PoWa cobot family – a name that symbolizes its powerful, industrial-grade performance in a compact collaborative robot form.”
The new PoWa family addresses a long‑standing gap in the market between traditional cobots, that often lack the speed and payload required for industrial applications, and conventional industrial robots, which are designed for highly specialized, large-scale automation environments, going beyond the needs of many collaborative tasks.
PoWa extends ABB Robotics’ comprehensive cobot offer with industrial-grade performance including six different payload categories, from 7kg to 30kg, the longest reach and highest arm load on the market and best-in-class top speed of up to 5.8 m/s.*

Purpose-built for compact environments and ideally suited for applications such as high-speed machine tending, palletizing, screwdriving and arcwelding, PoWa enables manufacturers to automate heavier and faster processes, while maintaining the flexibility, ease of use and compact footprint of collaborative robotics.
PoWa cobots are exceptionally easy to use, through programmable buttons on the arm-side interface and no-code programming and are compatible with an extensive ecosystem of third-party accessories. PoWa can be unboxed and operational within an hour and enables seamless plug-and-play with a wide range of tools, blending industrial-grade connectivity and performance with collaborative robot flexibility.
Powered by the ABB OmniCore controller platform, the new PoWa cobots deliver best-in-class motion control, speed, and precision and can be integrated with ABB Robotics’ expanding suite of AI-powered software, including Robot Studio® and Wizard Easy Programming, enabling intuitive programming, fast deployment and maximum uptime.
Ensuring collaborative robots can do more things, in more places, and do it faster, safer and smarter is part of ABB Robotics vision for more autonomous and versatile robotics (AVRTM). By developing a new generation of intelligent, flexible, adaptative, and collaborative multi-skilled robots, ABB Robotics furthers robots’ ability to learn, understand and plan independently, giving them greater autonomy and versatility.

* Speed of PoWa™ 10 and PoWa™ 13
ABB Robotics as one of the world’s leading robotics companies, is the only company with a comprehensive and integrated AI-powered portfolio covering robots, cobots and Autonomous Mobile Robots (AMRs), designed and orchestrated by our value-creating software. We help companies of all sizes and sectors - from automotive to electronics and logistics – to outperform by becoming more resilient, flexible and efficient. ABB Robotics is at the forefront of developing and commercializing a new generation of Autonomous Versatile Robotics (AVR), leading a global innovation ecosystem of partners in advancing efficient hardware and intelligent software with industrial performance. The business employs approximately 7,000 people. go.abb/robotics
-
ABB Robotics Global Media Relations
Email: rory.smith@gb.abb.com
Phone: +447548780120