ABB IE6 SynRM motors deliver a major boost for industrial energy efficiency
Press release
- ABB IE6 Hyper-Efficiency SynRM motors are now available in large frame sizes across a wide power range from 110 to 450 kW
- Operators gain a 76 percent improvement1 in energy savings, ROI and CO2 emissions when they choose IE6 instead of an IE5 motor
- SynRM magnet-free technology offers a sustainable solution designed for recyclability and no use of rare earth metals
ABB is accelerating industrial energy efficiency with its expanded range of IE6 Hyper‑Efficiency synchronous reluctance (SynRM) motors. This magnet‑free technology—now available from 110 to 450 kW in frame sizes 280 and 315, and speeds up to 3600 rpm—brings next-level efficiency and sustainability to even more industrial applications. This move builds on the 2024 milestone when ABB was the world’s first manufacturer to launch a magnet‑free IE6 SynRM motor for specialist applications. ABB has now made this breakthrough its mainstream option, moving ahead of the anticipated IE6 Hyper‑Efficiency standard.
“The IEA’s World Energy Outlook 20252 reinforces energy efficiency as one of the fastest, and most cost‑effective levers for industrial productivity and decarbonization. In line with our Engineered to Outrun philosophy, the IE6 Hyper‑Efficiency SynRM motors are designed exactly for this moment,” said Stefan Floeck, President IEC LV Motors, ABB. “Customers can now access world‑leading efficiency across a wider power range, often achieving payback in just months while moving closer to their sustainability targets.”
Switching to IE5 Ultra-Premium efficiency SynRM motors is proven to deliver major savings compared to an equivalent IE4 induction motor package. However, there is an even greater benefit when stepping up to ABB’s now-standard IE6 SynRM option. Over a typical 20-year service life, the savings3 are increased to €51,200 and 92,200 kg CO2— equivalent to 21.5 gasoline-powered passenger vehicles driving for one year. That represents an additional 76 percent improvement than when upgrading from IE5 to IE6, with an ROI of eight months.

ABB IE6 Hyper-Efficiency SynRM, family range 
ABB IE6 Hyper-Efficiency SynRM, large frames, from 110 to 450kW 
SynRM Rotor 
ABB IE6 Hyper-Efficiency SynRM motor and Drive 
ABB IE6 SynRM motors and Drives in pumping application
Designed with sustainability at the core, the IE6 SynRM contains no permanent magnets or rare earth metals, is 98 percent recyclable, and forms part of the ABB EcoSolutions™ portfolio with fully verified Environmental Product Declarations (ISO 14025 Type III). This enables customers and partners to make more informed, sustainable choices through increased transparency about each product’s circularity and environmental impact.
The IE6 SynRM motors match the size of standard induction motors, making them a simple drop‑in replacement for fans, pumps, compressors and other applications. As a perfect pairing with an ABB variable speed drive (VSD), they reinforce ABB’s commitment to breakthrough energy efficiency, reduced operating costs, and helping industries accelerate their decarbonization journey.
To learn more about ABB’s SynRM motors, visit this website.
1 - Substituting an IE4 induction motor with an IE5 SynRM could avoid annual CO2 emissions of 2,610 kg. With ABB’s IE6 SynRM as the standard option, this increases to 4,610 kg - a 76 percent improvement.
2 - IEA (2025), World Energy Outlook 2025, IEA, Paris https://www.iea.org/reports/world-energy-outlook-2025, License: CC BY 4.0 (report); CC BY NC SA 4.0 (Annex A).
3 - Calculation based on a 110 kW motor application with a 8760 hour running time at 75 percent power and an assumed energy cost of €0.2 per kWh
ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and around 110,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com
ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing and circular solutions for customers, industries and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun – leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on over 140 years of domain expertise in electric powertrains, our more than 23,000 employees across 100 countries learn and improve every day. go.abb/motion
Related Links
IE6 Hyper-Efficiency SynRM motors
IE5 and IE6 SynRM motors - Product Page
Downloads
ABB_IE6_SynRM_Product Family.png
-
Media Motion
Email: media-motion@ch.abb.com